This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x norFlash启动

Other Parts Discussed in Thread: SN74AVC32T245

The Fast External boot feature:
• Consists of a blind jump in ARM mode to address 0x08000000 in an external XIP device connected to
CS0
• The jump is performed with minimum on-chip ROM Code execution (only configures GPMC interface),
without configuring any PLL
• Allows the customer to create its own booting code
• Is set up by means of the configuration pins, see Table 26-7.
Addr/Data muxed device or a non-muxed (selected using SYSBOOT[11:10]) device in connected in
XIP_MUX2 configuration
• Bus width selected by SYSBOOT[8]
• CS0 chip select
• No wait monitoring is available

你好,我看到AM335xdatasheet这样介绍的(红色部分),我目前XIP启动,并且是非复用 norFlash启动,按照红色描述应该按照XIP_MUX2连接,对吗?GPMC_ADVN_ALE这个信号时地址锁存线有什么作用?,在gpmc不用这个线行吗?在table26-9表中看到BE1N在模式XIP_MUX2中为什么要连接GPMC_CSN2 and GPMC_BE1N?

  • 现在AM335X上设计nor flash启动的相关要点总结如下,供大家参考。

    1. 关于nor flash启动的信息

    可以参考TRM的26.1.7.2 XIP Memory章节,在这里就不详述了。

    2. 设计时注意点

    由于AM335X的管脚有限,所以在应用中许多客户会考虑采用GPMC数据线/地址线复用的方式连接外部的nor flash。这样可以将GPMC_AD[15:0]即作为16bit数据线,又作为低16bit的地址线。

    那在这种情况下,针对具体设计,需要注意哪些地方?

    在上述应用中,GPMC_AD会从即作为16bit数据线,又作为低16bit的地址线;从TRM的Table 7-5. GPMC Pin Multiplexing Options表格中可以知道,GPMC_A[10:1]会作为nor flash的高位地址线。而GPMC_A[10:1]存在两种复用方式,即可以将AM335X的pinmux mode0的这一组pin复用为GPMC_A[10:1],也可以将另一组复用为GPMC_A[10:1]。

    Signal ZCZ Pin Map(Pinmux mode0 ) ZCZ Pin Map (Pinmux mode1 )
    GPMC_A1 V14 R2
    GPMC_A2 U14 R3
    GPMC_A3 T14 R4
    GPMC_A4 R14 T1
    GPMC_A5 V15 T2
    GPMC_A6 U15 T3
    GPMC_A7 T15 T4
    GPMC_A8 V16 U5
    GPMC_A9 U16 R5
    GPMC_A10 T16 V5

    针对上述的两种连接,设计原理图时,需注意。

    (1)采用pinmux mode0组的连接时,需注意

        (a)latch需要采用上升沿锁存的,而不能使用电平锁存的。这是由于AM335x内的ROM CODE在nor flash启动时,有一组固定的GPMC时序。

        (b)高位地址线需要作下拉处理。由于ROM CODE在nor flash启动时,只对GPMC_AD[15:0]进行了初始化,而未对GPMC_A[10:1]进行。如果需要ROM CODE在启动初期时能够正确看到nor flash的地址空间,需要对高位地址线作下拉处理。

    (2) 采用pinmux mode1的连接时,需注意

    由于此时GPMC_A[10:1]与LCD_DATA复用,而LCD_DATA又在启动初期作为SYSBOOT管脚使用,在其管脚上会根据启动序列的选择存在相应的上下拉。这就与(1)中要求的nor flash启动初期需要对GPMC_A[10:1]一直保持下拉存在冲突。所以在这种应用下,需要增加一个bus transceiver对两者进行隔离。见下图。

    由于SYSBOOT的管脚状态只有在PORz的上升沿才会读取。而warm reset的输入管脚nRESET_OUT会在PORz完成后持续一段时间低电平,可参考TRM的Figure 8-19. PORz。所以可以通过此信号来作为Bus transceiver的控制信号。当nRESET_OUT为低时,根据SN74AVC32T245的逻辑,连接在总线上的信号会是A到B,期间PORz信号的上升沿触发时段,可以读取SYSBOOT的管脚状态。当nRESET_OUT持续一段时间低电平后,其电平会变为高,此时Bus transceiver则会将A侧的GPMC_A[10:1]与B侧SYSBOOT的上下拉隔离开。



    软件方面:

    在SDK-05.06.00.00及之后的版本的U-boot中已经添加了Nor flash启动的代码。在使用时,需要注意

    nor flash为XIP memory,其启动时不需要将SPL拷贝到RAM中运行,而可以直接在nor flash进行。由于nor flash启动,ROM CODE只对低16位地址进行了初始化,所以启动时只能访问0x08000000起始的64K x 16bit的地址空间。在此初始化中,u-boot.bin会执行对nor flash高位地址的初始化,以便后续AM335X能访问nor flash的整个地址空间。

    在u-boot/board/ti/am335x/board.c中的s_init函数中有对高地址线进行初始化的代码:

    #ifdef CONFIG_NOR_BOOT

    asm("stmfd      sp!, {r2 - r4}");

    asm("movw       r4, #0x8A4");

    asm("movw       r3, #0x44E1");

    asm("orr        r4, r4, r3, lsl #16");

    asm("mov        r2, #9");

    asm("mov        r3, #8");

    asm("gpmc_mux:  str     r2, [r4], #4");

    asm("subs       r3, r3, #1");

    asm("bne        gpmc_mux");

    asm("ldmfd      sp!, {r2 - r4}");

    #endif

    在选择上述表中的pinmux mode 1时,即nor flash的高位地址线连接的GPMC_A[10:1]是pinmux mode1组对应的管脚,则u-boot中不需要做修改。而如果连接的是表中的pinmux mode 0组对应的管脚,即需要修改代码如下:

    #ifdef CONFIG_NOR_BOOT

    asm("stmfd      sp!, {r2 - r4}");

    asm("movw       r4, #0x844"); Start point Change from LCD_DATA1 to GPMC_A1

    asm("movw       r3, #0x44E1");

    asm("orr        r4, r4, r3, lsl #16");

    asm("mov        r2, #8"); Change #9 to #8, GPMC_A1 to GPMC_A11 as mode0

    asm("mov        r3, #11"); Change #8 to #11, because there are 11 lines.

    asm("gpmc_mux:  str     r2, [r4], #4");

    asm("subs       r3, r3, #1");

    asm("bne        gpmc_mux");

    asm("ldmfd      sp!, {r2 - r4}");

    #endif

    另外,对应上述两组不同的连接时,SYSBOOT对应的设置也不相同。如选择pinmux mode0组的连接,则需要配置SYSBOOT,选择XIP(mux1)或者XIP(mux1) w/WAIT0启动。而选择pinmux mode1时,则需要配置SYSBOOT,选择XIP(mux2)或者XIP(mux2) w/WAIT0启动。



  •  你好,很感谢你的回答,还有一点没有理解,就是在模式1时为什么配置8个寄存器?我项目目前用32M的norflash,谢谢!

    #ifdef CONFIG_NOR_BOOT

    asm("stmfd      sp!, {r2 - r4}");

    asm("movw       r4, #0x8A4");

    asm("movw       r3, #0x44E1");

    asm("orr        r4, r4, r3, lsl #16");

    asm("mov        r2, #9");

    asm("mov        r3, #8");  为什么只配置8个寄存器?

    asm("gpmc_mux:  str     r2, [r4], #4");

    asm("subs       r3, r3, #1");

    asm("bne        gpmc_mux");

    asm("ldmfd      sp!, {r2 - r4}");

    #endif