This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在《AM437x Sitara Processors》P106,看到RTC的供电电流分别为2ma(典型电压值为1.1V ),5ma(典型电压值为1.8V)
在TI的GVM原理图上可以看到,这个两个电源是使用BAT和主电源进行供电的,如果需要长时间单独使用BAT进行供电,按3V纽扣电池容量约500mah,那么采用电阻分压的方式,提供者两路电源,只能供个三、四天,请问如何解决这个问题,RTC的实际电流是多少,有没有个典型值?谢谢。
您好
根据TI_AM437x_EVM参考设计,我们自行设计一套板卡,RTC供电的配置与参考设计一致。CPU的RTC系统的1V8,1V1由TPS65218的VDD5 ,VDD6供电,使用内核4.9.65版本进行测试,发现RTC掉电后的供电电流一开始是10uA,2min左右突然升高为60uA,然后一直保持着60uA,请问TI是否有对新版本内核也进行测试过RTC的供电电流呢?
由于急于需要帮客户解决,希望能够尽快得到您的回复,谢谢!