您好,我参考的是http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/46608.aspx,已经显示Nor programming complete successfully,但是关电重新拨码,无法boot成功。请问怎么检查错误。
看0X800000000的空间,断电之后和断电之前地址里的东西不一样。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我参考的是http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/t/46608.aspx,已经显示Nor programming complete successfully,但是关电重新拨码,无法boot成功。请问怎么检查错误。
看0X800000000的空间,断电之后和断电之前地址里的东西不一样。
谢谢
断点后需要拨码为ROM SPI boot,EVM设置为:SW3 OFF ON OFF OFF, SW4:ON ON ON ON, SW5:ON ON OFF ON, SW6: ON ON ON ON
在重新设置拨码开关后,等待一会后通过ccs链接仿真器,查看此时的pc停留的位置,看PC是否执行到应用代码,如果还在0x20b00000的地址段则说明还停留在RBL中运行,在memory browser中输入0x1087fffc查看改地址对应的value是否为程序入口地址(入口地址可在map中查看对应c_int00)