在开发产品中我们使用的PHY芯片是IP101GR,但是在TI提供的开发软件中菜单里没有支持这颗芯片的初始化程序。故而造成产品中的网口无法正常使用。请教各位如果不想改动硬件的情况下,是否可以将IP101的LINUX环境下初始化代码移植到软件里就可以了吗?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在开发产品中我们使用的PHY芯片是IP101GR,但是在TI提供的开发软件中菜单里没有支持这颗芯片的初始化程序。故而造成产品中的网口无法正常使用。请教各位如果不想改动硬件的情况下,是否可以将IP101的LINUX环境下初始化代码移植到软件里就可以了吗?谢谢
一般的phy应该是通用的啊,处理好PHY ID就应该可以互换啊。
请问这个PHY,以及PHY和MAC的连接方式相比开发板的有什么不同吗???