This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713烧写hex文件到flash问题



各位老师,我仿照别人的烧写程序改写了一个自己的hex文件烧写程序,DSP是DSP6713,Flash是AM29LV160D,程序是从hex文件中每次读取10行,对这10行进行处理主要是去掉空格和换行符等,然后将其烧写进FLASH,之后再读取10行,循环进行直到读完整个hex文件。现在的问题是:我的进行完第一次10行的读取烧写后,到第二次就会挂死在那里,始终没找到原因,希望大家帮忙看看这是怎么回事?


下面是程序代码:
——————————————————————————————————————————

#include "Sun6713_config.h"
#include <csl_chip.h>

#include <math.h>



#define Sourceaddr   0x90000000

Uint8  Tempdata[720];
Uint8  Tempdata2[740];
Uint16 Tempdata1;
unsigned short Data_to_write[120];
unsigned char Data_from_flash[1024];
char           filename[128];
long           codelength;
long           datalength;         
long           lengthtemp;
unsigned int  processaddr=Sourceaddr;
unsigned int   counter=0;


/********************************************************************************/
volatile Uint16* FLASH_ADR1 = (volatile Uint16 *)(0x90000000+(0x555<<1));
volatile Uint16* FLASH_ADR2 = (volatile Uint16 *)(0x90000000+(0x2AA<<1));
#define  Pass_Flag   0
#define  Fail_Flag   1 
#define                FLASH_UL1        0x012a;//0xAA
#define                FLASH_UL2        0x0095;//0x55
#define                FLASH_UL3        0x0100;//0x80
#define                FLASH_UL4        0x012a;//0xAA
#define                FLASH_UL5        0x0095;//0x55
#define                FLASH_SECTOR_UL6        0x30
#define                FLASH_CHIP_UL6                0x0010;//0x10
#define                FLASH_PROGRAM        0x0120;//0xA0
#define                SECTOR_SIZE        0x8000
#define                BLOCK_SIZE        0x8000
#define                CHIP_SIZE        0x40000

void flash_chip_erase()
{    
  *FLASH_ADR1=FLASH_UL1;//0xaa;    (volatile Uint16*)
  *FLASH_ADR2=FLASH_UL2;//0x55;(volatile Uint16*)
  *FLASH_ADR1=FLASH_UL3;//0x80;(volatile Uint16*)
  *FLASH_ADR1=FLASH_UL4;//0xaa;(volatile Uint16*)
  *FLASH_ADR2=FLASH_UL5;//0x55;(volatile Uint16*)
  *FLASH_ADR1=FLASH_CHIP_UL6;//0x10;   (volatile Uint16*)
}  

int Write_Flash_Word(Uint16 *data,Uint16 *address)

  *(volatile Uint16 *)FLASH_ADR1=FLASH_UL1;//0xaa;
  *(volatile Uint16 *)FLASH_ADR2=FLASH_UL2;//0x55;
  *(volatile Uint16 *)FLASH_ADR1=FLASH_PROGRAM;//0xa0;
  (*address)=*data; 
  //return(Toggle_Bit_Check(address));
  return Pass_Flag;
}

int Read_Flash_Word(Uint16 *data,Uint16 *address) 
{  
  *(volatile Uint16 *)FLASH_ADR1=FLASH_UL1;//0xaa;
  *(volatile Uint16 *)FLASH_ADR2=FLASH_UL2;//0x55;
  *(volatile Uint16 *)FLASH_ADR1=0x01b0;//0xf0;
  *data=(*address); 
  //return(Toggle_Bit_Check(address));
  return Pass_Flag;


void Write_Flash(Uint16 Data_to_write[],Uint16 *write_address) 

  int j;  
  for(j=0;j<120;j++)
   Write_Flash_Word(&Data_to_write[j],write_address++);  
}

/********************************************************************************/
main()
{        

/*******************************************************/
/***        hex文件下载到Flash                ***/
        FILE *stream;
        long int datalength1;
        long codelength1;
        int  i,k;
        int Conditionback=1;  

        /* Initialize DEC6713 board. */
        DSP6713_Init();

        puts("Please Input your file\n");
        scanf("%s",filename);
        
        flash_chip_erase(); 
        puts(" erasing the Flash\n");
        stream=fopen(filename,"rb");
        fseek(stream,0,SEEK_END);          /* the end address of the file */
        codelength1 = (long)ftell(stream);
        fseek(stream,0,SEEK_SET);          /* the start address of the file */
        datalength1 = (long)ftell(stream);
        codelength = codelength1-datalength1;/* calculate the length of the file */
        
        if(stream != NULL)
        {  
           while(Conditionback)
           { 
             if(codelength>740)
               {
                 datalength    = 740;         
                 codelength   -= 740;
                 lengthtemp    = 740;
               } 
             else
               {
                 datalength    = codelength;
                 lengthtemp    = codelength;
                 Conditionback = 0;
               }
             fread(Tempdata2,sizeof(unsigned char),datalength,stream);
             /************************/
             /************************/
             if(datalength<740)
             {
               for(i=datalength;i<740;i++)
               {
                 Tempdata2='F';
               }
             }
             /************************/
             /************************/             
         for(k=0;k<10;k++)
             {  
               for(i=0;i<72;i++)
               {
                 Tempdata[72*k+i]=Tempdata2[74*k+i];
               }
             }
             /************************/
             /************************/         
    for(i=0;i<720;i++)
             {
               switch(Tempdata)
               {
                 case'0':Tempdata=0x00;break;
                 case'1':Tempdata=0x01;break;
                 case'2':Tempdata=0x02;break;
                 case'3':Tempdata=0x03;break;
                 case'4':Tempdata=0x04;break;
                 case'5':Tempdata=0x05;break;
                 case'6':Tempdata=0x06;break;
                 case'7':Tempdata=0x07;break;
                 case'8':Tempdata=0x08;break;
                 case'9':Tempdata=0x09;break;
                 case'A':Tempdata=0x0A;break;
                 case'B':Tempdata=0x0B;break;
                 case'C':Tempdata=0x0C;break;
                 case'D':Tempdata=0x0D;break;
                 case'E':Tempdata=0x0E;break;
                 case'F':Tempdata=0x0F;break;
                 default:break;
               }
             }
         for(i=0;i<120;i++)
             {
             
               Data_to_write=(Tempdata[i*6]<<12)|(Tempdata[i*6+1]<<8)|(Tempdata[i*6+3]<<4)|Tempdata[i*6+4];
             
             }

    
            Write_Flash(Data_to_write,(Uint16 *)processaddr);
                
         processaddr += 120;
         printf("%s,%d\n","Writing FLASH is in progress",counter++);
       }
       fclose(stream);
       *(unsigned char *)Sourceaddr = 0xF0;       
       puts(" End of writting the Flash\n");
       puts(" Now Please reset your system\n");
    }
    else
       puts("the file is empty\n");

}

/*******************************************************/