This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678的SPI BOOT是否需要IBL的介入?



1、之前按照版上的SPI BOOT单核启动的例子,在EVM上成功实现了单核的SPI BOOT,虽然过程中不涉及到EEPROM中的IBL,但我不能确定IBL是否有参与。现在自己画了一块板子,用的是PG2.0的6678芯片,板子上没有挂EEPROM,只挂了一块SPI Flash,现在板子还没到,看了一些帖子,现在有些担心能否用SPI成功BOOT。

2、另外在多核boot的时候,了解到存在两种方法,一种是使用MAD工具;另一种是在先前单核Boot的基础上,将多个boot table通过merge工具合成一个table,然后依旧按照单核boot的流程。而MAD工具好像是会涉及到IBL的,不知道是否无法在我的板子上实施?走第二种方式是否可以绕过IBL?

3、还有一个问题,在部署多核BOOT的之前,使用同一份代码如何生成8核各自的.out文件?如果8核需要执行不同的代码,那在生成对应的Image的时候,又该如何?我的理解是,不管是一份Image还是多份,都是通过配置.cmd文件,来指定各核的内存分配,最后链接生成不同的image,不知道是否理解正确?