我现在采用的平台是DM8168 EVM,但是由于客户需要,我们需要自己制作一个FPGA的视频采集板卡用于外部视频的输入采集(原因由于和DM8168的接口不一致)。
现在我们不知道怎么采集从fpga传入到DM8168的视频数据流,利用OMX里面的例子程序capture_encoder例子,但是采集不到任何数据,输出文件大小始终是为0Byte。
请问我们需要写VIN0的采集驱动模块吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
368是通过ISP的并口接bt656的,8168没有isp,不能从isp并口接入,只能需要通过VP口来接bt656数据,请参考DVR的参考设计。
谢谢你的回复.
我现在碰到的问题就是,摄像机的分辨率不够高,而我老板想做成5M的像素,所以我想到了直接将MT9P031来连接DM8168,但是不行
1 我在看文档的时候,8168 没有给出与sensor直接的对接,但是类似的方案在dm365的reference design 上看到,可能就是上面说的8168没有ISP的缘故
2 不能对接的原因是什么,如果是数据格式不一致的话能不能通过FPGA来实现转换,即sensor和8168中间添加FPGA来转换格式
3 如果是电气特性导致的,该怎么来解决
最近这段时间看文档很迷茫,谢谢指导啊
1,你可以用8127来做,8127是带isp可以接5M的raw sensor,编码加速器性能也用,用8168太浪费了。
2.实在想用8168来做你还得去找带isp功能的fpga把RAW经过转成YUV,
貌似8168的hdvpss的VIN只有1080p的capture能力(待确认),如果这样你需要自己在DDR里把图像拼起来然后送去编码,又是麻烦事。