使用Tera Term通过UART下载u-boot.min.uart时,如果parity设置成even时,无法下载,如果设置成none就可以下载进去。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
http://processors.wiki.ti.com/index.php/TI81XX_PSP_UBOOT_User_Guide#U-Boot_UART_support
这里提到要设置成NONE的啊。。。
Chris Meng,谢谢你的回答!
我尝试过在串口打印CCC全部结束后,再下载uboot min,并且配置成了uart bootmode,同样是不行的。另外,我又用了一个接有4片16位DDR2的板子,不过数据线只接了24位,下载成功了,但是并未显示“TI-MIN#”。我在CCS上调试好像总结出DSP的DDR MAP是在EMIF0和EMIF1上每隔128字节交叉访问的,因为我原来的板子只在DDR1上接了两片16位的DDR2,所以我想是不是需要修改程序的硬件配置,即uart.min的源程序。如果是的话,请问改在RDK里的那个文件里修改?
Han Weikun,
帖子里提到的DDR2是否是笔误?你使用的是DDR3对么?
你使用的接口是EMIF0还是EMIF1? wiki上的补丁应该是针对使用EMIF0的。
Han Weikun,
1. 补丁使用的是EMIF0,而你使用的是EMIF1,需要做调整
2. 默认软件使用的都是DDR3,可以使用DDR2,但DDR的配置你需要调整。
我下载还是只停在1024字节的位置,我用的两片DDR2的型号是IS46DR16640B,都接在EMIF1上,片选都用DDR1_CS0。我具体做法是:打完补丁,在include/configs/ti8148_evm.h里使能#define CONFIG_TI814X_EMV_DDR2;修改u-boot/arch/arm/include/asm/arch-ti81xx/ddr_defs_ti814x.h文件(将USE_EMIF1定义1,MIN_DMM_LISA_MAP_3定义为0x80400200);修改u-boot/board/ti/ti8148/evm.c,改为当USE_EMIF1=1时将MIN_DMM_LISA_MAP_3赋给DMM_LISA_MAP_3,不行,又尝试将MIN_DMM_LISA_MAP_3赋给DMM_LISA_MAP_2,还是不行。
请问我哪里改错了或忘记改了?