This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678能否在运行中动态改变主频和停用ddr



问题描述:当前我们的应用中,6678使用中有一段时间处于休眠状态,只需要emif运行。希望能在此时尽量降低功耗。因此考虑在这段时间降低主频,并停用ddr。 1,6678是否允许在运行过程中重新配置pll以修改主频?应当如何操作? 2.6678能否运行中通过psc动态将ddr下电,之后再上电?操作要注意什么吗?
  • 可以动态重配PLL,但是EMIF DDR控制器 PSC的状态是always on,不能软件关掉。

  • 您好:

            1、动态重配PLL的操作是否与第一次初始化流程完全一样?有无特殊要求?

            2、之前已经初始化好(并可能进行了初始化操作)的外部通信接口,包括PCIE SRIO HYPERLINK EMIF16以及DDR3这些端口会不会受到什么影响?是否都需要重新配置呢?

             3、如果我将DDR PLL设置为bypass模式,不向其提供高频时钟,是否允许?能不能达到节省功耗的效果呢?

              谢谢!