This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6670的CACHE性能



您好!

我现在在用TMS320C6670,在用到cache的时候有一些疑惑,希望您能给予解答。

1.L1 cache的数据位宽为64位,而6670里有32个16位乘法单元,那么当调用乘法单元的时候一次最多只能够给4个乘法单元提供数据,那么怎么才能把32个同时调用起来呢?

2.我看C6670手册里提到,在1.2GHz的情况下,定点可以达到38.4GMacs/Core,浮点可以达到19.2GFlops/Core的性能,可是在实现的时候发现根本无法达到这个数值,而且按照目前cache的位宽也没法达到这个数值啊,这个数值是怎么来的,怎么做才能把性能提高到实现标称值呢?

希望能尽快得到您的回答,谢谢!!