This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678上电复位的问题



您好,

     新做的板子,利用FPGA给6678进行上电复位操作,按照 6678 datasheet  7.1的Core Before IO Power Sequencing的顺序对6678进行上电复位操作。仅涉及PORn,RESETFULLn,RESETn三个信号。

    问题:DSP的RESETSTATn信号始终保持低电平,SYSCLKOUT无时钟,没有复位成功?

  • 你的现象是没有复位成功,最好再检查一下时序和电压时钟的输入

  • 您好,我们用示波器测量了一下PORn,RESETn,RESETFULLn三个信号,测量结果是: RESETn先变高电平,等待300us左右,PORn变高,等待17us后RESETFULLn变高。

    测量点是这三个信号从FPGA输出到DSP时的下拉电阻处。

    这三个信号测得的这个时序有没有问题?手册上只提到了最短时间100us和24个时钟周期。

    这三个信号输入电流有没有影响?