This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于DM8127的NAND FLASH,有两个问题请教一下:
1、DM8127的NAND FLASH是否最大支持512MB的FLASH?
2、DM8127的NAND FLASH接8位的NAND FLASH是不是有不确定的问题出现?我咨询代理商,他们说接8位的NAND可能有问题,他们没有这么接过,他们推荐使用16bit的NAND。请帮我确认一下。
3、我们的PCB为了节省空间,只想用两片16bit的内存,也就是只连接DDRC0控制器,总容量为1GB,另外一个DDRC1不连接,请问将来跑linux系统和DSP算法同时运行,这样设计能否满足要求?
希望大家给予帮助,谢谢大家了。
nan han 说:关于DM8127的NAND FLASH,有两个问题请教一下:
1、DM8127的NAND FLASH是否最大支持512MB的FLASH?
【Chris】请参考TRM里面的NAND ID列表Table 4-14. Supported NAND Devices,最大NAND是64Gb,也就是8GB。
nan han 说:2、DM8127的NAND FLASH接8位的NAND FLASH是不是有不确定的问题出现?我咨询代理商,他们说接8位的NAND可能有问题,他们没有这么接过,他们推荐使用16bit的NAND。请帮我确认一下。
【Chris】请使用Table 4-14. Supported NAND Devices里面提到的NAND。
nan han 说:3、我们的PCB为了节省空间,只想用两片16bit的内存,也就是只连接DDRC0控制器,总容量为1GB,另外一个DDRC1不连接,请问将来跑linux系统和DSP算法同时运行,这样设计能否满足要求?
1、芯片手册中的这一句是什么意思?“512MB of address space divided among up to 8 chip selects.最大存储数据BGB是怎么计算出来的呢?
2、如果接8位的NAND FLASH,是接DM8127的GPMC的高8位还是低8位?请问您见过的产品中,有没有使用8位的NAND?我问了几个人,他们都使用的参考板的16位的NAND。
请帮我解答一下吧,非常感谢。
1. 可以。
2. 我暂时没听说过8位存在你说的问题。 不过仍然会推荐16bit。
3. DM8127的两个DDR控制器,去掉一个就会去掉一半的DDR吞吐带宽,这个是增加DDR容量也不能弥补的,三思三思,也省不掉很多空间的。
nan han 说:1、芯片手册中的这一句是什么意思?“512MB of address space divided among up to 8 chip selects.最大存储数据BGB是怎么计算出来的呢?
线性寻址,也就是一个地址,一个内容是按照这样计算的,例如Nor flash。NAND flash是通过命令访问的,不是线性寻址。