Dear all:
目前采用DM385芯片做外同步采集,时钟,HS,VS,DE,信号的频率都对,信号质量也正常,却产生over flow这个问题,目前想要了解该接口的时序图,请问题谁有?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all:
目前采用DM385芯片做外同步采集,时钟,HS,VS,DE,信号的频率都对,信号质量也正常,却产生over flow这个问题,目前想要了解该接口的时序图,请问题谁有?谢谢!
Hi ,
如我前面帖子回复中所说,时序图就是DM385手册里面的那个timing。
请问那张图有什么地方不清楚的?
Hi, 时序已经找到,已经通过示波器测量波形正常,另外我采用tvp7002芯片输出24bit,RGB给dm385的采集口,时钟中间通过电平转换芯片,sn74avc16t245-q1,这个是否会有影响?谢谢!
Hi,
1、 时序图VIN[X]A_CLK里面有clk-fld,实际上采集时候只用到clk,de,vs,hs,没有用到fld引脚,用原来的采集bsp包是否存有影响呢?
2、 时序图里面th(CLK-D)input hold time, data valid from VIN[x]A_CLK high/low -0.5ns,这个实际反映DE信号和CLK信号的走线关系是什么呢?dm8168的是0ns时候解释是数据线要比时钟线长。
Thanks
1. 你没有用到隔行,FID不必考虑。
2. 这个还是要通过实测来看时序是否满足的。 我记得你之前好像已经reverse过tvp7002的输出时钟了?
推荐的接法还是用YUV422 Embedded Sync