各位老师:
我想请问一下,在ipnc_rdk_v3.8中关于REV1与REV2主要区别是什么呢?
我们自己做的DM385的板子,仿照的是之前appro的板子,在开发板开发的时候,我用的是3.5的ubl,uboot以及kernel和文件系统。但是我们新作的板子只能用3.8编译的REV2选项的ubl,uboot才能跑起来(其他的都不行REV1,Binary目录下的,3.5,3.0都不可以)。可能是什么原因呢?还请各位老师帮忙分析一下!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位老师:
我想请问一下,在ipnc_rdk_v3.8中关于REV1与REV2主要区别是什么呢?
我们自己做的DM385的板子,仿照的是之前appro的板子,在开发板开发的时候,我用的是3.5的ubl,uboot以及kernel和文件系统。但是我们新作的板子只能用3.8编译的REV2选项的ubl,uboot才能跑起来(其他的都不行REV1,Binary目录下的,3.5,3.0都不可以)。可能是什么原因呢?还请各位老师帮忙分析一下!
If the GND is pin 3, it is Rev 1.
您好,您参考的是Appro的那个相机吗?
如果是的话,你的意思是你的用的是rev1的板子,但是只有rev2的代码可以跑?
是的,appro385的相机,所以我也觉得很奇怪,不知道是不是硬件有了问题!