This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【求助】关于(638K2K )TCP处理开销差异较大问题?



在6638K2K EVM板上测试TCP处理能力,发现TCP-2与其它3个差别很大:

单独启动TCP-2处理一个5969的CB块,需要近55000circle;

但分别单独启动TCP-0、1、3,处理5969的CB,只需要不到20000circle。

麻烦TI技术工程师能提供一些解答,或者思路和提示。

谢谢~

  • 4个TCP3D是完全一样,由于不同TCP3D所使用的EDMA channel会不一样,所以测试的性能会有所差异,你可以试试连续处启动处理多个CB看看性能的差异变化。

    我觉得即使EDMA通道不一样,性能有所差异,但是不应该差距那么大,麻烦描述一下你的测试方法,是只有TCP3D工作么,有没有可能是其他诸如EDMA 通道冲突影响引入delay呢。