This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助C5515支持NAND Flash的问题



各位TI专家好:

    我想实现一个低功耗数据采集和存储项目,想采用C5515DSP作为主处理器,使用NAND Flash作为存储介质,数据采集完成之后通过USB2.0 High Speed上传数据。

    由于数据容量比较大,可能需要采用16GByte左右的NAND。我对C5515的EMIF对NAND Flash的支持不是很清楚,我看到CSL_emif_nand范例代码中设备枚举中最大只有2GB,每页2KB。

    但是我找到的大容量的16GB NAND都是4K每页MCL NAND,不清楚C5515是不是支持这种NAND,是否需要修改CSL代码。

    能否提供C5515能够支持的NAND Flash的参考。

   另外,是否有USB2.0 MSC读写NAND的速度的参考资料

    谢谢!