This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6747的USB的几个问题?



现在正在调试C6747的USB,在TI网址看了许多资料,感觉目前开发USB好像必须使用BIOS,于是,下载了PSP和USBBIOS,发现里面的程序都是HID或者MSC的,我们的应用仅仅是向PC发一些简单的数,PC上编写上位机程序,收到后再做处理,我们这里有用FT245或CY68013的,现在想直接用C6747的USB。但是现在感觉无从下手。有几个问题想请教:

1.有没有不是基于BIOS的USB程序例子?

2.仅仅是向PC发一些简单的数的话,是不是需要使用USB的Communication Device Class,而不是HID或MSC,那么是不是需要windows的驱动,驱动哪儿可以获得?
谢谢