This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 Public ROM启动了哪些外设?



最近在看有关DM8168的TRM

Chapter25提到Boot的事宜

我想知道以下问题:

1:Figure 25-1中所提到的片内核外的外设是否都由Public ROM完成驱动?

2:Image Shadowing中提到U-Boot镜像不能超过255KB,是不是意味着在DM8168中,

   不需要把U-Boot转存到外部的DDR这一步骤,而在片内的L3 RAM中就可以完成全部的Boot流程?

3:U-Boot需要完成哪些片内外设的驱动?

4:Linux Kernel中提供了哪些驱动?

 

初来乍到,概念混乱,请不吝赐教,谢谢!