This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: ARM(A15)与DSP(C66x)通信的IPC应用

Part Number: AM5718

TI工程师您好,

       最近在应用am5718这块芯片的核间通信,关于ARM与DSP之间通过IPC消息机制来进行通信,

根据Processor SDK Linux  for AM57X 08_02_01_00上3.6.3中提到需要LINUX和RTOS SDK的版本号必须保持一致,但是我发现am5718的Linux的08版本的两个版本号与RTOS的对不上

Linux的08版本是:08.02.01.00和08.02.00.04

RTOS的08版本是:08.01.00.09

较低版本倒是有能对应上,但是我们目前板子的Linux系统就是08.02.01.00的,如果RTOS用08.01.00.09是否会影响arm与dsp通信不上呢?

Best Regards
Ling Wang