This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: 一直显示:"Encountered a problem loading file: xxx.out Could not open file"

Part Number: TMS320C6657


我现在经常使用的是PDK,但是在调TI给的upp_loopback_noOs例程的时候,发现它使用了mcsdk,所以我在D盘下面装了一个mcsdk

现在的情况是build已经通过,但是debug的时候,一直报错:C66xx_0: GEL: Encountered a problem loading file: F:\workspace\mproj\upp_mcsdk\upp_loopback_noOS\Debug\upp_loopback_noOS.out Could not open file(F:\workspace\mproj是我的workspace),想请问有没有人知道该怎么解决这种问题?

另外,最近一直在调UPP和FPGA的通讯,却停在了第一步。之前用EMIF,UPP和EMIF的差别还是挺大的,所以先在网上找了一些例程,TI论坛里的一些demo和我的情况不符,有两点:

1)组件包不一样,像TI给的例程也是用MCSDK,但是我需要PDK

2)有报错can't resolve name (xdc.bld.ITarget3),可以参见我上一篇提问TMS320C6657: CCS报错can't resolve name - 处理器论坛 - 处理器 - E2ETm 设计支持 (ti.com)

如果有同行也在研究UPP和FPGA,可以加好友一起讨论,谢谢!~