This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: edma的使用

Part Number: TMS320C6678

您好,在参考pdk_c667x_2_0_16\packages\ti\csl\example\edma下的edm_tset例程,设置PaRAM部分如下,其中对ACNT设置为256,BCNT设置为1,CCNT设置为1,使用A传输方式,根据对手册的理解,srcBidx=dtsBidx=ACNT,scrCidx=dstCidx=ACNT,但是例子中并不是这么设置的,是理解的有问题么?

myParamSetup.option = CSL_EDMA3_OPT_MAKE(CSL_EDMA3_ITCCH_DIS, \
CSL_EDMA3_TCCH_DIS, \
CSL_EDMA3_ITCINT_DIS, \
CSL_EDMA3_TCINT_EN, \
0, CSL_EDMA3_TCC_NORMAL,\
CSL_EDMA3_FIFOWIDTH_NONE, \
CSL_EDMA3_STATIC_DIS, \
CSL_EDMA3_SYNC_A, \
CSL_EDMA3_ADDRMODE_INCR, \
CSL_EDMA3_ADDRMODE_INCR );
myParamSetup.srcAddr = (Uint32)srcBuff1;
myParamSetup.aCntbCnt = CSL_EDMA3_CNT_MAKE(256,1);
myParamSetup.dstAddr = (Uint32)dstBuff1;
myParamSetup.srcDstBidx = CSL_EDMA3_BIDX_MAKE(1,1);
myParamSetup.linkBcntrld= CSL_EDMA3_LINKBCNTRLD_MAKE(hParamPong,0);
myParamSetup.srcDstCidx = CSL_EDMA3_CIDX_MAKE(0,1);
myParamSetup.cCnt = 1;