This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXEVM6678LE 用xds560v2-USB Mezzninie Emulator 无法connect

Other Parts Discussed in Thread: TMS320C6678

1,

2,

 

3,上电一分钟后launch 4,connect  出错

(no boot sw3(off  on on on)  sw4(on on on on)   sw5(on on on off)   sw6(on on on on) )

  • 您好,

    1. 确认USB与上面的子板USB口连接;

    2. 修改为no boot mode:sw3(off  on on on)  sw4(on on on on)   sw5(on on on on)   sw6(on on on on)

  • 我也有遇到这一情况,有时候会发生找不到DNUM的错误,就算连接时没有报错,也无法查看寄存器的值,随后的load program时也会报错,提示找不到IER。个人感觉可能是在读取寄存器值时出了问题。

    似乎这与软件安装的方法也有关系。

    win7 64bit下 ccs5.1装在非系统盘无以上错误,但编译sys/bios例程时永远卡在49%。

    ccs5.0.3不管装在什么位置都会有上述错误,无解。

    难道真的只有在XP下才能较完美的运行?(用XP系统测试的确没有异常)

  • 我修改了 boot mode  

    connect 还是出错

     

    我的.ccxml 文件<?xml version="1.0" encoding="UTF-8" standalone="no"?>
    <configurations XML_version="1.2" id="configurations_0">
    <configuration XML_version="1.2" id="Blackhawk XDS560v2-USB Mezzanine Emulator_0">
            <instance XML_version="1.2" desc="Blackhawk XDS560v2-USB Mezzanine Emulator_0" href="connections/BH-XDS560v2-USB_Mezzanine.xml" id="Blackhawk XDS560v2-USB Mezzanine Emulator_0" xml="BH-XDS560v2-USB_Mezzanine.xml" xmlpath="connections"/>
            <connection XML_version="1.2" id="Blackhawk XDS560v2-USB Mezzanine Emulator_0">
                <instance XML_version="1.2" href="drivers/tixds560icepick_d.xml" id="drivers" xml="tixds560icepick_d.xml" xmlpath="drivers"/>
                <instance XML_version="1.2" href="drivers/tixds560c66xx.xml" id="drivers" xml="tixds560c66xx.xml" xmlpath="drivers"/>
                <instance XML_version="1.2" href="drivers/tixds560cs_dap.xml" id="drivers" xml="tixds560cs_dap.xml" xmlpath="drivers"/>
                <platform XML_version="1.2" id="platform_0">
                    <instance XML_version="1.2" desc="TMS320C6678_0" href="Devices/C6678.xml" id="TMS320C6678_0" xml="C6678.xml" xmlpath="Devices"/>
                    <device HW_revision="1" XML_version="1.2" description="C66x core" id="TMS320C6678_0" partnum="TMS320C6678">
                        <router HW_revision="1.0" XML_version="1.2" description="ICEPick_D Router" id="IcePick_D_0" isa="ICEPICK_D">
                            <subpath id="subpath_0">
                                <cpu HW_revision="1.0" XML_version="1.2" description="C66xx CGEM+FP CPU" id="C66xx_0" isa="TMS320C66XX">
                                    <property Type="filepathfield" Value="..\..\emulation\boards\evmc6678l\gel\evmc6678l.gel" id="GEL File"/>
                                </cpu>
                            </subpath>
                        </router>
                    </device>
                </platform>
            </connection>
        </configuration>
    </configurations>

  • 我的ccs5.0.3 装在系统盘 XP系统这有问题吗  非系统盘我也试过不行

  • 您好,

    请对照附件EVM技术手册观察一下EVM母版的LED情况,以确定EVM板正常;同时对照下述描述观察XDS560v2子板的LED情况,确定子板是否正常。如果子板异常,请尝试将子板卸下来,然后使用EVM板集成的XDS100V1仿真器看看是否有问题。谢谢

    TMDXEVM6678L_Technical_Reference_Manual_2V00.pdf