Other Parts Discussed in Thread: THS8200, TVP7002
目前我们用AM335X外接THS8200输出通用VGA接口(TTL电平转成模拟信号),现在想外接TFT屏,想把VGA模拟信号转成TTL电平。能否有专用芯片,求推荐一款,以及其电路图,谢谢啦。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有点没太明白,你们想接TFT屏的话,直接用RGB565,或者RGB888的接口可以吗?AM335x大部分客户接的TFT屏都是这样的接口。如果是想做一个兼容设置(既要VGA又要RGB),用GPIO做一个swtich控制开关呗。
有点没太明白你上面描述的应用场景。为啥要先THS8200,再转一下?TFT的接口是什么样的?
如果您是为了长距离的考虑,建议您参考我们的lvds芯片,可以联系我们当地的代理商或者销售
我们,我的控制系统已经用THS8200转换成VGA接口(没有TFT的接口),现在我要使用的是TFT屏,所以需要一款VGA信号转TTL信号的芯片,可以推荐一款吗?
我们,我的控制系统已经用THS8200转换成VGA接口(没有TFT的接口),现在我要使用的是TFT屏,所以需要一款VGA信号转TTL信号的芯片,可以推荐一款吗?
情况是这样的,我们现在 的板卡已经留出VGA接口了,也就是说我已经用THS8200将RGB565(LCD16)转换为VGA信号了,但是我们客户有现成TFT屏,所以我想做个转接板,讲VGA模拟信号转换成LCD信号,供TFT屏使用。你们能提供一款专用芯片吗?将RGB模拟信号转换成TTL信号,不知道我说清楚了没有?
TVP7002 能提供下原理图吗?和THS8200的接口对应的原理图。
Hi TVP7002 就是把THS8200反过来用的一个芯片。 THS8200是RGB/YUV -> VGA, TVP7002是VGA -> RGB/YUV 的
产品主页:
http://www.ti.com.cn/product/cn/TVP7002?keyMatch=TVP7002&tisearch=Search-CN
http://www.ti.com.cn/tool/cn/TVP7002EVM?keyMatch=TVP7002&tisearch=Search-CN
参考原理图请看:
http://www.ti.com/cn/lit/pdf/sleu098
参考寄存器配置请看:
http://www.ti.com/cn/lit/zip/slec029
BR,
Eason
一些常见疑问可以看这里
http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/52747.aspx