This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x 1GHz下解码视频死机

Other Parts Discussed in Thread: AM3354

你好,我们现在正在用AM3354的1GHz版本芯片开发HMI系统,客户要求能够播放简单的视频文件,分辨率小于640*480,通过播放软件解码播放没有多长时间(大概几秒钟)就会出现死机的情况,概率100%。而如果降频到800Mhz以后,死机的情况就没有了。我们之前已经通过论坛提供的工具对DDR进行了SW leveling。可以确认的是AM3354在1Ghz的情况下,运行大部分应用没有出现过死机的情况,只有在播放视频时会出现,请问这种情况如何解决?谢谢!

  • 想确认一下:你们目前使用的1GHz电源解决方案是使用TI推荐的PMU吗?具体的是哪个?我想排除一下,会不会是在系统loading过高时,由于电源问题导致的这个问题。

    从你描述的情况上来说,如果跑在800MHz确认是没问题的,那么应用软件上面的因素就可以排除了,在1GHz时候出问题,我个人更倾向于查driver部分的配置以及对1GHz的电源供电情况。driver部分如果是使用较新版本的SDK的话,应该是OK的, 比如SDK6.0;电源方面,就需要查一下VDD_MPU,VDD_CORE这两路是否在datasheet要求的范围之内了。