This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SDK: Processor SDK Linux for J721e 08_06_01
已經編譯完成,並燒入到SD可以進入系統。
----
目前打算新增layer,
$ cd /ti-processor-sdk-linux-j7-evm-08_06_01_02/yocto-build
$ . ./sources/oe-core/oe-init-build-env
$ bitbake-layers create-layer meta-stressapptest
但是發生問題如下圖,
後來有修改toolchain_base_path。但是因為缺少 gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi
還是無法產生新的 meta-stressapptest。
NOTE: Starting bitbake server...
ERROR: Unable to start bitbake server (None)
ERROR: Server log for this session (/home/macon/works/jacinto7/j721e_evm/linux/20230521_08_06_01_02/ti-processor-sdk-linux-j7-evm-08_06_01_02/yocto-build/build/bitbake-cookerdaemon.log):
--- Starting bitbake server pid 3440 at 2023-06-06 17:06:14.944751 ---
ERROR: Failed to obtain external Arm toolchain version: Execution of '/home/macon/works/jacinto7/toolchain/gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi/bin/arm-none-linux-gnueabi-gcc -v' failed: command not found
--------
之前根據 document,只需要2個 toolchains。
gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu.tar.xz
gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf.tar.xz
這邊想請問2個問題,
1, 能否移除gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueabi 需求,如果是的話,請問如何修改?。
2. 如果否,請問哪邊可以下載 gcc-arm-9.2-ti2020.01-armv5-x86_64-arm-none-linux-gnueab。
謝謝。
您好,您的问题我们需要升级到英文论坛看下,链接如下,有答复尽快给您。