Part Number: TDA4VM
Other Parts Discussed in Thread: J721EXENETXPANEVM, J7EXPCXEVM
您好
我们采购了一块扩展板(OPN# J7EXPC01EVM),直接装到评估板上,使用评估板出厂自带的SD启动,发现网口不能用。是否需要另外操作来匹配该扩展板,比如说有对应的设备树文件等,或者有扩展板的使用说明么?祝好!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Other Parts Discussed in Thread: J721EXENETXPANEVM, J7EXPCXEVM
您好
我们采购了一块扩展板(OPN# J7EXPC01EVM),直接装到评估板上,使用评估板出厂自带的SD启动,发现网口不能用。是否需要另外操作来匹配该扩展板,比如说有对应的设备树文件等,或者有扩展板的使用说明么?祝好!
两块网络扩展板我们都采购了,分别是J721EXENETXPANEVM,J7EXPCXEVM。安装到评估板之后都不可以直接使用。
&cpsw0 {
/*
* Disable cpsw0 since cpsw9g_virt_mac is the default Ethernet
* controller. cpsw0 is enabled with overlay for native
* Ethernet driver support.
*/
status = "disabled";
};
这个cpsw0对应的是哪个板子,然后另一块需要如何做才能使用,当前评估板共有十个网口,当前只有MCU ENET是可以使用的
您好,您的问题我们需要升级到英文论坛看下。由于假期在即,我们可能无法及时向您转达新的信息,您可以点击以下链接来查看最新进展:
您好,
能否分享下 Linux terminal log (from Main UART0 i.e. logs from A72) 和 Ethfw log (from Main UART2 i.e. logs from MCU2_0 (Main R5F0_0))
您能否根据SDK Documentation确认 EVM 的硬件连接?
请问使用的SDK 版本是?