一直没弄懂。当我的硬件有DSP,m4要跑sys/bios然后mpu跑的是linux,怎样把bios加载到DSP或m4,以及XDCTtools和linux,sys/bios三者之间的关系也没弄懂
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请参考:http://processors.wiki.ti.com/index.php/SysLink_Overview#What_is_SysLink.3F
SysLink is runtime software and an associated porting kit that simplifies the development of embedded applications in which either General-Purpose microprocessors (GPP) or DSPs communicate with each other. The SysLink product provides software connectivity between multiple processors. Each processor may run either an HLOS such as Linux, QNX, etc. or an RTOS such as SYS/BIOS. In addition, a processor may also be designated as the master for another slave processor, and may be responsible for controlling the slave processor's execution (including boot-loading the slave).
The SysLink product provides the following services to frameworks and applications:
SYS/BIOS operating system is expected to be running on the slaves with all of these platforms.
Target configurations: SysLink provides reusable & portable modules for:
要想跑起来syslink,A15跑LINUX或者SYSBIOS,其他核跑SYSBIOS
AM57XX的文件系统下/lib/firmware/dra7-dsp1-fw.xe66这个就是DSP的程序,你可以把你的程序替换上去就行了