This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6747: EDMA传输问题

Part Number: TMS320C6747


提前对您的支持表示感谢,我还在尝试EDMA来搬运数据,现在我使用region的ESR和ICR可以实现触发,表现为运行的时候,相应的寄存器EDMACC0_CCSTAT 在0x00000110和ox0之间跳转,这说明TR已经传输,并且通道也开始工作,并且IPR = 0x00000001,这是否已经说明EDMA完成了传输的所有的流程,但是我在目标地址没有看到搬运来的数据,后面我将源地址进行修改,都在L2上进行搬运,目的地址还是没有对应的数据,我将代码附在下面,希望得到您的支持~

初始化代码

void COhwDMAInit(void)
{
    unsigned int count = 0;
   // General EDMA Initial  memory protection is unlocked
    MPPA0 = 0x000004B3;
    MPPAG = 0x000004B3;

   /* Step 1: EDMA initialization */
   QUEPRI	=	0x10;    //芯片级设置  ok
   QWMTHRA =(16<<8u)|(16 & 0xFF);   //ok


   /* Clear the Event miss Registers   */
   EMCR =  0xFFFFFFFF;              //事件丢失寄存器清除  No
   EMCRH = 0xFFFFFFFF;              //  NO
   QEMCR =  0xFFFFFFFF;            //No

   /* Clear CCERR register                                                 */
   CCERRCLR =  0xFFFFFFFF;      //No

   /* FOR TYPE EDMA*/
   /* Enable the DMA (0 - 64) channels in the DRAE and DRAEH register   shadow region open */
   DRAE1 = 0xFFFFFFFF; //影子区域  如果配置了则需要操作影子区域的寄存器来实现控制   Yes
   DRAEH1 =0xFFFFFFFF;     //NO

   /* Step 2: Programming DMA Channel (and Param set) */

   /* All events are one to one mapped with the channels  64个事件 64个通道 事件映射通道 */
   DCHMAP0 = 0 <<5;                                // 0 event mapped with the channel   No
   DCHMAP1 = 1 <<5;                                // 1 event mapped with the channel   NO
   DCHMAP2 = 2 <<5;                                // 1 event mapped with the channel  No


   DMAQNUM0=0x0;        //全部放在队列0中进行   Yes


//   EESR =0x20000000;    //29
//   COhwDMA_Disable();

   return;
}

参数集设置代码  其中up和down数据都在0x008位置内,

void COhwDMA_rxConfig()
{
   

    /*----------------------------------------------------------------------*/
    /* Initialize EDMA for Receive Samples for RX0                          */
    *(volatile uint32_t *) (EVENT1_PARAMS + EDMA_PARAMS_OPT )  = 0x0010000C; //| (1<<12) ;            选择AB传输 防链接  Yes
    *(volatile uint32_t *) (EVENT1_PARAMS + EDMA_PARAMS_SRC )  =(uint32_t)&COexEmOutPktBuf.up;		//   L2的0x            yes(uint32_t)COexSqInputPtr
    *(volatile uint32_t *) (EVENT1_PARAMS + EDMA_PARAMS_CNT )  = (0x00120000 | 0x00000002);  			// in bytes   BCNT ACNT   yes  2A
    *(volatile uint32_t *) (EVENT1_PARAMS + EDMA_PARAMS_DST )  =  (uint32_t)&COexEmInPktBuf.dn;                      		// Dst      Yes   (uint32_t)&COexEmInPktBuf.dn;
    *(volatile uint32_t *) (EVENT1_PARAMS + EDMA_PARAMS_IDX )  = (0x00020000 |0x00000002);                //dstcidx  srccidx   yes
    *(volatile uint32_t *) (EVENT1_PARAMS + EDMA_PARAMS_LNK )  = 0x0000FFFF;    // null                   //Bcntrld       yes
    *(volatile uint32_t *) (EVENT1_PARAMS + EDMA_PARAMS_CIDX)  = 0;                                       //
    *(volatile uint32_t *) (EVENT1_PARAMS + EDMA_PARAMS_CCNT)  = 0x00000001;   // Important!!!


}

采用CPU手动触发