This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: DSP配置为从EMIF NOR FLASH启动时,在线加载调试程序出现问题

Part Number: TMS320C6678


调试程序时,FPGA配置DSP为从EMIF NOR FLASH启动,该FLASH挂在FPGA上。在EMIF FLASH的前1K字节保存了一段搬移程序,在CCS进行CPU/SYSTEM reset后,看到核0的PC指针会跳到0x20B00000,0x70000034。当核0的PC地址为0x20B00000时,程序可以正常加载,当核0的PC地址为0x70000000开始的一段空间,加载程序失败,提示下面的错误。

所以,当从FLASH启动时,DSP内部是因为什么原因,导致加载程序出现上面的异常情况?

调试时,配置为NO BOOT启动,是为了保证程序正常加载?