This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-TDA4VM: SK-TDA4VM中使用ipc

Part Number: SK-TDA4VM

你好,我用SDK编译的vx_app_arm_ipc.out(在主函数中添加了打印信息),copy到板端后一直无法输出添加的printf打印信息。要如何才能正确的实现改过程呢?

  • 板卡:SK-TDA4VM

    SDK:ti-processor-sdk-rtos-j721e-evm-08_04_00_06

    image版本: 08.04.00.10

    操作:cd vision

              make sdk -j8

             cp vx_app_arm_ipc.out  ./rootfs/opt

              ./vx_app_arm_ipc.out

  • Hi :Team

    My steps are as follows:

    Flash prebuilt 8.4 EdgeAI SDK for SK-TDA4VM onto SD card
    Add a printf statement in the main function. Specifically: 
    Run the following commands to build and copy over file to SD card

    1999 cd vision_apps/
    2000 make sdk
    2001 sudo cp out/J7/A72/LINUX/release/vx_app_arm_ipc.out /media/anzhigang/rootfs/opt/
    2002 history

    sk-tda4vm development board operation as follows:

    root@tda4vm-sk:/opt/vision_apps# ./vx_app_arm_ipc.out
    APP: Init ... !!!
    MEM: Init ... !!!
    MEM: Initialized DMA HEAP (fd=4) !!!
    MEM: Init ... Done !!!
    IPC: Init ... !!!
    IPC: Init ... Done !!!
    REMOTE_SERVICE: Init ... !!!
    REMOTE_SERVICE: Init ... Done !!!
    380.945149 s: GTC Frequency = 200 MHz
    APP: Init ... Done !!!
    ...and the rest of the default printf logs from vx_app_arm_ipc.out


    Then,Two more questions,Need help answering:
    1、I added the print in your patch file and can see the output log normally?
    2、log output of the debug version is the same as that of the realese version?

    cherry,帮转到英文论坛,谢谢!!

  • 好的已跟进。

  • 您好,请看如下答复:

    1. You should see the exact same output as I was seeing. If the software is the same and the hardware is also the same, then I do not have a good idea on why there is a difference between our setup.
    2. The debug version should have more print statements, but the printf the expert added in the patch should work without building for the debug version.

    vx_app_arm_ipc.out - we attached vx_app_arm_ipc.out, but can you try running this? If you see "Testing printf" at the start of the logs, then there is something that is wrong with how printf is added to the code, or something wrong with the build. If there are no "Testing printf", we would suspect something wrong with the underlying image flashed onto the SD card.

  • Can you compile and run printf testing according to the printf testing I provided?I'd like to take a look at your log output。THS

  • Hi,

    I described in my post from July 24th the steps I have ran to compile and run printf test. I have also copied the relevant logs that shows that printf is functioning as expected.

    If you are following the steps exactly as described, then there should be no difference between our logs. However, looking through the steps that have been shared with me, it does look like the steps are followed but resulting logs are different.

    Because there are some differences in resulting behavior, I would like to make our setup as similar as possible by sharing my vx_app_arm_ipc.out that I have verified the extra printf is working. Please run the .out file in my previous post, and share logs so that we can narrow down whether the issue is in the underlying EdgeAI SDK image flashed onto the SD card, or an issue with the build environment/procedure.

    Thanks.