Part Number: TDA4VE-Q1
Other Parts Discussed in Thread: J721EXCPXEVM, J721S2XSOMXEVM
使用 通用处理器板J721EXCPXEVM 和 J721S2XSOMXEVM 板 ,pdk 版本 ti-processor-sdk-rtos-j721s2-evm-08_06_01_03。板子能够从sd卡启动,然后我进入uboot使用sf命令刷写norflash,然后调整拨码开关从norflash启动,但是板子无法正常启动,电流只有0.43A,mcu,wakeup和main串口均无log打印。我已通过回读的方法检查过了flash中的内容与对应文件一致,请帮分析下无法启动的原因。
我刷写flash的内容是从pdk里面拿的,包括:
- sbl_ospi_img_hlos_mcu1_0_release.tiimage is flashed to address 0x0
- tifs.bin is flashed to address 0x80000
- sbl_baremetal_boot_test_j721s2_evm_all_coresTestApp_release.appimage is flashed to address 0x100000
- nor_spi_patterns.bin to 0x3fc0000
我的拨码开关是:
SW8: 00000000
SW9:01000000
SW3:0100001111