This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: 我使用edgeai_tidl_tools编译自己的onnx模型时,遇到如下错误,请问原因是什么?急!

Part Number: TDA4VM

 ************** Frame index 1 : Running float import *************
SUGGESTION: [TIDL_InnerProductLayer] Gemm_100 Size larger than 2048 * 2048 is not optimal.
SUGGESTION: [TIDL_InnerProductLayer] Gemm_102 Size larger than 2048 * 2048 is not optimal.
****************************************************
** 2 WARNINGS 0 ERRORS **
****************************************************
80.527042s: VX_ZONE_ERROR:[tivxAlgiVisionCreate:335] Calling ialg.algInit failed with status = -1110
80.527078s: VX_ZONE_ERROR:[tivxKernelTIDLCreate:720] tivxAlgiVisionCreate returned NULL
80.570362s: VX_ZONE_ERROR:[ownContextSendCmd:801] Command ack message returned failure cmd_status: -1
80.570377s: VX_ZONE_ERROR:[ownContextSendCmd:835] tivxEventWait() failed.
80.570379s: VX_ZONE_ERROR:[ownNodeKernelInit:527] Target kernel, TIVX_CMD_NODE_CREATE failed for node TIDLNode
80.570381s: VX_ZONE_ERROR:[ownNodeKernelInit:528] Please be sure the target callbacks have been registered for this core
80.570382s: VX_ZONE_ERROR:[ownNodeKernelInit:529] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel
80.570385s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 0, kernel com.ti.tidl:1:4 ... failed !!!
80.570388s: VX_ZONE_ERROR:[vxVerifyGraph:2055] Node kernel init failed
80.570390s: VX_ZONE_ERROR:[vxVerifyGraph:2109] Graph verify failed
TIDL_RT_OVX: ERROR: Verifying TIDL graph ... Failed !!!
TIDL_RT_OVX: ERROR: Verify OpenVX graph failed