This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6672: 如果我更换了NAND Flash后,在原来的烧写程序的工程中改哪些内容,以及post上电自检程序需要改吗。

Part Number: TMS320C6672


我更改了PLATFORM_DEVICE_info gDeviceNand = {0xC8, 0xAA, PLATFORM_DEVICE_NAND, 8, BLOCKS_PER_DEVICE, PAGES_PER_BLOCK, BYTES_PER_PAGE, SPARE_BYTES_PER_PAGE, PLATFORM_DEVID_NAND512R3A2D, 0, 2048, 0, NULL, NULL};还有

addr_cycle_stream[0] =
(uint8_t) BUILD_ADDR_ROW(COL(7), COL(6), COL(5), COL(4), COL(3), COL(2), COL(1), COL(0));

/* Col 2 - II cycle */
addr_cycle_stream[1] =
(uint8_t) BUILD_ADDR_ROW(LOW, LOW, LOW, LOW, COL(11), COL(10),COL(9),COL(8));

/* Row 1 - III cycle */
addr_cycle_stream[2] =
(uint8_t) BUILD_ADDR_ROW(BLOCK(1), BLOCK(0), PAGE(5), PAGE(4), PAGE(3), PAGE(2), PAGE(1), PAGE(0));

/* Row 2 - IV cycle */
addr_cycle_stream[3] =
(uint8_t) BUILD_ADDR_ROW(BLOCK(9), BLOCK(8), BLOCK(7), BLOCK(6), BLOCK(5), BLOCK(4), BLOCK(3), BLOCK(2));

/* Row 3 - V cycle */
addr_cycle_stream[4] =
(uint8_t) BUILD_ADDR_ROW(LOW, LOW, LOW, LOW, LOW, LOW, LOW, BLOCK(10));命令码都没有区别目前少些不进去