Other Parts Discussed in Thread: AM3352
在virtual box虚拟机中使用CCS10通过USB连接AM3352开发板,虚拟机USB设备识别到了开发板,但在CCS中想要通过USB对开发板进行烧录时失败,提示one of the ftdi driver functions used during the connect returned bad status or an error
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问电脑操作系统是什么?请看一下下面的网站。
https://software-dl.ti.com/ccs/esd/documents/ccs_vmware.html
请问用的是什么仿真器?有的支持得不好,请看上面网站上的说明。
When using Linux in a Virtual Machine, most of the details and supported debug probes above are applicable to this scenario. However, XDS100-class debug probes perform very slowly in this configuration, thus preventing any practical usage. XDS200 and XDS560v2 work fine when using Windows 7 as host operating system.
Also, Spectrum Digital debug probes are known to have problems in being properly initialized in Linux under VmWare, therefore avoid using them in such environments. The operation under Linux running natively does not have these issues.
Some people reported that XDS200 on Parallels (MacOS virtual machine) does not work when using Windows 7 as guest OS, but no tests were done.
请看下面e2e工程师的回复。
I assume the customer is running the Ubuntu in the virtual box?
I have occasionally seen some challenges related to connecting the virtual machine to the hardware ports on the computer. We will not be able to support questions specifically related to the virtual machine itself.
If the customer installed CCS with normal permissions (instead of elevated permissions with "sudo"), did they make sure to run the install_drivers.sh script after doing the installation? reference https://software-dl.ti.com/ccs/esd/documents/ccsv10_linux_host_support.html