This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: AM62A build linux SDK, Makefile.build: No such file or directory

Part Number: AM62A7


Hello TI,

This is the first time I used the SDK of the platform, a detailed use process was not found in the user manual.

My current operation steps are described as follows:

1.download SDK

2../ti-processor-sdk-linux-am62axx-evm-08.06.00.45-Linux-x86-Install.bin

3../setup.sh

4../linux-devkit.sh

5.make

and then, Makefile.build: No such file or directory

How can I solve this compilation and report error problem. hwo can I find Makefile.build this file.

In addition, are there any relevant use process documents? thanks.