TI 专家你好:
开发板:自己开发板
sdk: ti-processor-sdk-rtos-j721e-evm-08_01_00_13
我想在mcu1_0上去使用了 DM timer.

其中,周期配置为5000, 周期类型为 微秒(period_type= 0)。
但是在调试过程中,发现周期远远超过了5毫秒,然后我输出日志,
打印了定时器的配置:

发现周期参数不对。请问一下TI专家,怎么解决这个问题。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI 专家你好:
开发板:自己开发板
sdk: ti-processor-sdk-rtos-j721e-evm-08_01_00_13
我想在mcu1_0上去使用了 DM timer.

其中,周期配置为5000, 周期类型为 微秒(period_type= 0)。
但是在调试过程中,发现周期远远超过了5毫秒,然后我输出日志,
打印了定时器的配置:

发现周期参数不对。请问一下TI专家,怎么解决这个问题。
谢谢。
请看下面e2e工程师的回复。
Are they referring to any existing example. If yes, can you please share the changes that they have made so I can reproduce this error on my end?
/*
* \brief Main file for TI-RTOS build
*/
/* ========================================================================== */
/* Include Files */
/* ========================================================================== */
#include <ti/csl/arch/csl_arch.h>
#include <ti/csl/soc.h>
#include <ti/csl/cslr.h>
#include <ti/osal/osal.h>
#include <ti/osal/TaskP.h>
#if (defined (BUILD_MCU1_0) && (defined (SOC_J721E) || defined (SOC_J7200)))
#include <ti/drv/sciclient/sciserver_tirtos.h>
#endif
#include <ti/drv/ipc/include/ipc_rsctypes.h>
#include <Adc.h>
#include "AdcApp.h"
#include "string.h"
#include "app_utils.h"
#include "AdcApp_Startup.h"
#include <ti/board/board.h>
#include <ti/drv/sciclient/sciclient.h>
#include <ti/kernel/freertos/FreeRTOS-LTS/FreeRTOS-Kernel/include/FreeRTOS.h>
#include <ti/kernel/freertos/FreeRTOS-LTS/FreeRTOS-Kernel/include/task.h>
#include <ti/drv/sciclient/sciclient.h>
#include <ti/drv/sciclient/sciserver_tirtos.h>
#include "Dio.h"
#include "pmic_app.h"
#include "pmic_common.h"
#include "ipc_trace.h"
#include <ti/csl/arch/r5/csl_arm_r5.h>
/* ========================================================================== */
/* Macros & Typedefs */
/* ========================================================================== */
/* Test application stack size */
#define APP_TASK_STACK (10U * 1024U)
/**< Stack required for the stack */
/**< Task name */
#define APP_TSK_STACK_MAIN (32U * 1024U)
/**< Test application stack size */
#define IPC_INIT_SCISERVER_TASK_PRI (12)
#define APP_SCISERVER_INIT_TSK_STACK (32U * 1024U)
/* High Priority for SCI Server - must be higher than Low priority task */
#define IPC_SETUP_SCISERVER_TASK_PRI_HIGH (8)
/*
* Low Priority for SCI Server - must be higher than IPC echo test tasks
* to prevent delay in handling Sciserver requests when test is performing
* multicore ping/pong.
*/
#define IPC_SETUP_SCISERVER_TASK_PRI_LOW (7)
#define MSG_APP_NAME "adc_detect"
#define MSG_NORMAL 0x01U
#define ADC_INIT_TASK_PRI (3)
#define PMIC_TASK_PRI (5)
#define TISCI_DEV_MCU_ADC0 0
#define TISCI_DEV_MCU_ADC1 1
#define TISCI_DEV_MCU_I2C0 194
#define TISCI_DEV_WKUP_I2C0 197
#define TISCI_DEV_USB0 288
#define TISCI_DEV_MMCSD0 91
/* None */
/* ==========================================================================*/
/* Function Declarations */
/* ========================================================================== */
void CanProfile_setupSciServer(void);
void ipc_initSciclient(void);
void Ipc_setupSciServer(void);
/* ========================================================================== */
/* Global Variables */
/* ========================================================================== */
/* application stack */
static uint8_t CanApp_TaskStack[APP_TASK_STACK] __attribute__((aligned(32)));
static uint8_t SciServer_TaskStack[APP_TASK_STACK] __attribute__((aligned(32)));
static uint8_t gAppTskStackMain[APP_TSK_STACK_MAIN] __attribute__ ((aligned(8192)));
static uint8_t gSciserverInitTskStack[APP_SCISERVER_INIT_TSK_STACK] __attribute__ ((aligned(8192)));
static uint8_t gAdcInitTskStack[APP_SCISERVER_INIT_TSK_STACK] __attribute__ ((aligned(8192)));
static uint8_t gPmicInitTskStack[APP_TASK_STACK] __attribute__ ((aligned(32)));
static void taskFxn(void* a0, void* a1);
static void Adc_detect_Fxn(void* a0, void* a1);
static void Pmic_wdg_Fxn(void* a0, void* a1);
extern void pmic_wdg_app_runner(void);
/**
* Without this linux kernel can not boot.
*/
const Ipc_ResourceTable ti_ipc_remoteproc_ResourceTable __attribute__ ((section (".resource_table"), aligned (4096))) =
{
{
1U, /* we're the first version that implements this */
2U, /* number of entries in the table */
{
0U,
0U, /* reserved, must be zero */
}
},
};
/* ==========================================================================*/
/* This is for adc detect */
/* ========================================================================== */
static uint32_t AdcApp_procImplicitStop(const Adc_ConfigType *Adc_ConfigPtr, uint32_t groupId);
static void AdcApp_procIsr(uint32_t grpIdx);
uint32_t Adc_TestPassed = E_OK;
/**< App Result Status Flag */
uint32_t Adc_AppLoopCount = 5U;
/**< Number of times App runs */
Adc_ValueGroupType Adc_AppBuffer[ADC_MAX_GROUP][
ADC_APP_BUF_SIZE_WORD];
/**< SetUp Result Buffer passed to driver */
Adc_ValueGroupType Adc_AppReadBuffer[ADC_MAX_GROUP][
ADC_APP_READ_BUF_SIZE_WORD];
/**< Output Result Buffer */
volatile uint32_t Adc_AppRdBufCount[ADC_MAX_GROUP];
/**< No of Samples Counter */
volatile uint32_t Adc_AppGroupDone[ADC_MAX_GROUP];
/**< Group Conversion Completion flag */
extern const Adc_ConfigType *Adc_ConfigPtr;
#define GET_ADC_VOITAGE(adcValue) (((adcValue)*(1800U)) / (4095U))
static SemaphoreP_Handle Pmic_Handle = NULL;
static TimerP_Handle dmhandle = NULL;
typedef struct Adc_Target
{
Adc_HWUnitType Adc_id;
uint16_t Channel;
uint32_t Voltage;
Adc_ValueGroupType Adc_Result;
} Adc_Target_t;
Adc_Target_t Adc_target = {
.Adc_id = ADC_UNIT_1,
.Channel = 1,
.Adc_Result = 0,
.Voltage = 0
};
/* ========================================================================== */
/* End of adc detect */
/* ========================================================================== */
int32_t local_moduleClockEnable(uint32_t moduleId)
{
int32_t retVal = 0;
int32_t status = -1;
uint32_t moduleState = 0U;
uint32_t resetState = 0U;
uint32_t contextLossState = 0U;
/* Get the module state.
No need to change the module state if it
is already ON
*/
status = Sciclient_pmGetModuleState(moduleId,
&moduleState,
&resetState,
&contextLossState,
SCICLIENT_SERVICE_WAIT_FOREVER);
if(moduleState == TISCI_MSG_VALUE_DEVICE_HW_STATE_OFF)
{
status = Sciclient_pmSetModuleState(moduleId,
TISCI_MSG_VALUE_DEVICE_SW_STATE_ON,
(TISCI_MSG_FLAG_AOP |
TISCI_MSG_FLAG_DEVICE_RESET_ISO),
SCICLIENT_SERVICE_WAIT_FOREVER);
if (status == 0)
{
status = Sciclient_pmSetModuleRst (moduleId,
0x0U,
SCICLIENT_SERVICE_WAIT_FOREVER);
if (status != 0)
{
retVal = -1;
}
}
else
{
retVal = -1;
}
}
return retVal;
}
TaskP_Handle task;
TaskP_Params taskParams;
int main(void)
{
/* Relocate FreeRTOS Reset Vectors from BTCM*/
void _freertosresetvectors (void);
memcpy((void *)0x0, (void *)_freertosresetvectors, 0x40);
OS_init();
/* Initialize the task params */
TaskP_Params_init(&taskParams);
/* Set the task priority higher than the default priority (1) */
taskParams.priority = 2;
taskParams.stack = gAppTskStackMain;
taskParams.stacksize = sizeof (gAppTskStackMain);
task = TaskP_create(taskFxn, &taskParams);
if(NULL == task)
{
OS_stop();
}
OS_start(); /* does not return */
}
static void tick_fxn(unsigned int t)
{
// Test here
}
static void taskFxn(void* a0, void* a1)
{
#ifdef UART_ENABLED
AppUtils_Init();
#endif
/* Initialize SCI Client - It must be called before board init */
ipc_initSciclient();
TaskP_Handle sciserverInitTask;
TaskP_Params sciserverInitTaskParams;
/* Initialize SCI Client Server */
TaskP_Params_init(&sciserverInitTaskParams);
sciserverInitTaskParams.priority = IPC_INIT_SCISERVER_TASK_PRI;
sciserverInitTaskParams.stack = gSciserverInitTskStack;
sciserverInitTaskParams.stacksize = sizeof (gSciserverInitTskStack);
sciserverInitTask = TaskP_create(Ipc_setupSciServer, &sciserverInitTaskParams);
if(NULL == sciserverInitTask)
{
OS_stop();
}
// Board_initCfg boardCfg;
// boardCfg = BOARD_INIT_PINMUX_CONFIG |
// BOARD_INIT_UART_STDIO;
// Board_init(boardCfg);
#if 1
TimerP_Params dmtimerPar;
TimerP_Params_init(&dmtimerPar);
dmtimerPar.period = 5000;
dmtimerPar.periodType = (uint32_t)TimerP_PeriodType_MICROSECS;
dmhandle = TimerP_create(TimerP_ANY, tick_fxn, &dmtimerPar);
if (NULL == dmhandle)
pmic_log_info("Creat dmtimer error.\n");
TimerP_start(dmhandle);
#endif
}
void ipc_initSciclient(void)
{
int32_t ret = CSL_PASS;
Sciclient_ConfigPrms_t config;
/* Now reinitialize it as default parameter */
ret = Sciclient_configPrmsInit(&config);
if (ret != CSL_PASS)
{
AppUtils_Printf(MSG_NORMAL, MSG_APP_NAME "Sciclient_configPrmsInit Failed\n");
}
#if (defined (BUILD_MCU1_0) && (defined (SOC_J721E) || defined (SOC_J7200) || defined (SOC_J721S2)))
if (ret == CSL_PASS)
{
ret = Sciclient_boardCfgParseHeader(
(uint8_t *)SCISERVER_COMMON_X509_HEADER_ADDR,
&config.inPmPrms, &config.inRmPrms);
if (ret != CSL_PASS)
{
AppUtils_Printf(MSG_NORMAL, MSG_APP_NAME "Sciclient_boardCfgParseHeader Failed\n");
}
}
#endif
if (ret == CSL_PASS)
{
ret = Sciclient_init(&config);
if (ret != CSL_PASS)
{
AppUtils_Printf(MSG_NORMAL, MSG_APP_NAME "Sciclient_init Failed\n");
}
}
}
void Ipc_setupSciServer(void)
{
Sciserver_TirtosCfgPrms_t appPrms;
int32_t ret = CSL_PASS;
ret = Sciserver_tirtosInitPrms_Init(&appPrms);
appPrms.taskPriority[SCISERVER_TASK_USER_LO] =
IPC_SETUP_SCISERVER_TASK_PRI_LOW;
appPrms.taskPriority[SCISERVER_TASK_USER_HI] =
IPC_SETUP_SCISERVER_TASK_PRI_HIGH;
if (ret == CSL_PASS)
{
ret = Sciserver_tirtosInit(&appPrms);
}
if (ret == CSL_PASS)
{
AppUtils_Printf(MSG_NORMAL, MSG_APP_NAME "Starting Sciserver..... PASSED\n");
}
else
{
AppUtils_Printf(MSG_NORMAL, MSG_APP_NAME "Starting Sciserver..... FAILED\n");
}
return;
}
2,将编译出来的固件,将其make u-boot-a72的 DM,编译tispl.bin
(注意:我在tick_fxn中,没有加入我们的代码,TI的专家可以将tda4vm板中的某一个IO作为测试点,将其5ms一次 循环拉高、拉低。通过示波器观察)

上述就是我用示波器测量的结果。时钟会在上电之后不久,会出现一次或多次挂死现象,待linux kernel启动完成后,就不会出现上述现象,且时钟稳定。麻烦TI专家帮忙分析一下。谢谢。
抱歉回复晚了,请看下面工程师的回复。
The timer configuration looks fine.
Do you see the same issue when just running the RTOS alone, without running the Linux on A72?
Also, can you try using any other timer instance and see if the results are same?
1,CCS debug的时候,是正常的(我想ccs去debug的时候是没有运行linux的)
2,我尝试过其他的DM timer ,但是毫无意外,均在linux kernel启动过程中,出现了这个问题。
同时,mcu 能使用的DM timer 不多, 即使TRM上有众多DM timer可以使用(大约20个),但是mcu能使用的也才几个,如下:
后来我尝试去修改这个mask,将其扩展为(0xFF),但是也有几个DM timer会创建不成功。
请问TI专家,您在开发板上,通过编译修改tispl.bin测试了这个DM timer了嘛?
结果是正常的嘛?