This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: SRIO 通信问题

Part Number: TMS320C6678

方案是用FPGA端采用NWIRTE-R格式向DSP端写入数据,DSP接收到数据采用REPSONE WITH DATA返回数据及运行状态。现在DSP端在裸核下采用SRIO的Direct I/O 方式控制LSU寄存器,其中设置了Ftype=Srio_Ftype_REPSONE;ttype=Srio_Ttype_Response_RESPONSE_PAYLOAD方式能否通过CSL的  CSL_SRIO_SetLSUTransfer(hSrio, LSU_Number, &tparams)函数实现RESPONE with data数据发送。

DSP在进行内回环测试过程,先通过进行NWIRTE-R的数据写入,然后再进行Srio_Ttype_Response_RESPONSE_PAYLOAD的写入,现在NWIRTE-R发送成功了,但是Response with data的事务发送时,CSL_SRIO_GetLSUCompletionCode(hSrio, LSU_Number, transactionID,&uiCompletionCode, &context)返回错误uiCompletionCod=-4状态,错误原因可能是是包类类型不支持,或者出现了对至少一个LSU的编码是无效的。

相关代码:

 /* wait loopback complete time set as 10ms, base on cpu freq as 1000MHz */
              timeout = 10000000;
              /* 1.3 caculate the read and write buffer for srio transfer address */
              //1.3计算srio传输地址的读写缓冲区
              srio_trans_src = (uint32_t *)t_buff_global;
         //     srio_trans_dst = (uint32_t *)r_buff_global;
             srio_trans_dst= (uint32_t  *)TARGET_ADDRESS;
             printf("NREAD  srio_trans_src= %d,srio_trans_dst=%d\n",srio_trans_src , srio_trans_dst);
            printf("NREAD  srio_trans_src= 0x%x,srio_trans_dst=0x%x\n",srio_trans_src , srio_trans_dst);
              //cuix add r_buff
              /* 1.4 set transfer parameters, srio nread test, devmem_buff -> r_buff */
              memset((void *)&tparams, 0, sizeof(tparams));
              tparams.rapidIOLSB = (uint32_t)srio_trans_src;
              tparams.dspAddress = (uint32_t)srio_trans_dst;
              tparams.bytecount = transfer_size;
              //Srio_Ftype_RESPONSE I/O Transaction

             //Ftype:w_format_type=Srio_Ftype_RESPONSE (13)  ttpye:Srio_Ttype_Response_RESPONSE_PAYLOAD(8)
            tparams.ftype = Srio_Ftype_RESPONSE ;           //Format fType
             tparams.ttype =Srio_Ttype_Response_RESPONSE_PAYLOAD ;

              //id of the target device to be sent
              tparams.dstID = REMOTE_DEVICEID1_8BIT;
              tparams.outPortID = SRIO_PORT;
              tparams.idSize = 0;
              /* wait LSU have available shadow register */
              while(1) {
                  if (CSL_SRIO_IsLSUFull (hSrio, LSU_Number) == FALSE)
                      break;
              }

              /* Get the LSU Context and Transaction Information. */
              CSL_SRIO_GetLSUContextTransaction(hSrio, LSU_Number,
                                                 &contextBit, &transactionID);
              transStart = _itoll(TSCH, TSCL);
              /* start srio transfer */
              CSL_SRIO_SetLSUTransfer(hSrio, LSU_Number, &tparams);

              /* wait for a transfer completion interrupt occur */
              while(timeout) {
                 CSL_SRIO_GetLSUCompletionCode(hSrio, LSU_Number, transactionID,
                                                  &uiCompletionCode, &context);
                 if(context == contextBit) {
                     /* disable pending transactions */
                     transactionID = 0xFF;
                     contextBit = 0xFF;

                     if(uiCompletionCode != 0) {
                          status = -1;
                          printf("SRIO transfer have error completed code %d\r\n", -(uiCompletionCode));
                          goto err_transfer;
                     }

                     break;
                 } else {
                      timeout--;
                      /* delay 1 cpu cyle */
                      asm (" nop");
                 }
              }

              if(timeout == 0) {
                  /* if transfer timeout occurs, return error status */
                  status = -1;

                  printf("SRIO transfer timeout\r\n");

                  goto err_transfer;
              }

              /* Calculate srio transfer used time */
              transCost = _itoll(TSCH, TSCL) - transStart;
              r_time = transCost;
              /* Calculate srio transfer read rate */
              //Srio_Ttype_Request_NREAD  读取数据
              r_rate = (float)transfer_size * main_pll_freq / r_time / 1024 / 1024 / 1024 * 8;
              w_rate_total += w_rate;
              r_rate_total += r_rate;
              for(i = 0; i < transfer_size; i++) {
                  printf("test addr: 0x%x, dst addr: 0x%x\r\n", \
                            w_buff_global[i], r_buff_global[i]);
                  if(w_buff_global[i] != r_buff_global[i]) {
                      printf(" src addr: 0x%x, dst addr: 0x%x\r\n", \
                                                   (uint32_t)&w_buff_global[i], (uint32_t)&r_buff_global[i]);
                      err_count++;
                      if(err_count == 1) {
                          printf("Frist Err occurred src addr: 0x%x, dst addr: 0x%x\r\n", \
                                      (uint32_t)&w_buff_global[i], (uint32_t)&r_buff_global[i]);
                          printf("dst val: 0x%x, ", r_buff_global[i]);
                          printf("expet val: 0x%x\r\n", w_buff_global[i]);
                      }
                  }

1.请教下,我们方案理论可行吗?但是TI的相关案例中,没有见过Response with data的事务发送的案例?

2.DSP端能采用SRIO采用Direct I/O的Srio_Ttype_Response_RESPONSE_PAYLOAD采用这个方式向FPGA的固定的地址写入数据?

3.如果可行,如何尝试修改uiCompletionCod=-4状态?

4.如果无法解答,能否帮我升级下可以?