1、DM385能用DVRRDK4.1来做开发吗?
2、板子的前端接的是两片解码芯片,通过DM385来进行采集;
3、如果可以使用,在RDK中涉及的DSP核部分的处理,需要改动的地方大吗?还是在rulesmake中修改为DM8107就可以了 ?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、DM385能用DVRRDK4.1来做开发吗?
2、板子的前端接的是两片解码芯片,通过DM385来进行采集;
3、如果可以使用,在RDK中涉及的DSP核部分的处理,需要改动的地方大吗?还是在rulesmake中修改为DM8107就可以了 ?
谢谢!
1. http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/385338.aspx You can follow this thread.
2. It is OK to capture 2 video streams from external video decoder
3. There is no DSP core in DM385/DM8107.
Please use IPNCRDK on DM385.
Why do you want to use DVRRDK on DM385?
Can IPNC RDK create GUI application or only web application?
No GUI integrated in IPNCRDK.
你可以用FBdev去画GUI
谢谢你的回答
但是我在 /dev底下没有看到fb啊?
我是手边是dm385红色相机那个rdk
请问它有其他的sdk可以用吗?
或是如何让一个linux console从hdmi显示出来?