This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6713的MCASP在I2S模式发送问题

大家好,我在使用C6713的MCASP时遇到这样的问题,使用EDMA的AXEVT0触发MCASP发送数据,当我把MCASP配置为突发模式(BURST)时能够正常发送数据,但是如果其他设置都不动,只将MCASP_AFSXCTL_XMOD_OF(0),改为MCASP_AFSXCTL_XMOD_OF(2)也就是改为I2S模式时,左右时钟能够正常产生,但是没有数据发出,不知道为什么?请各位大侠指点!

  • 我在想是不是需要用EDMA的AXEVTE0和AXEVTO0事件才行,我使用AXEVT0作为触发觉得EDMA只将第一个字节发送给MCASP,后面就没有再发送,因为一直没有产生EDMA发送中断,我如果改为BURST模式,就能够正常发送数据,EDMA也会正常产生中断,因为BURST模式DAC芯片不认识,只能接I2S模式,希望有经验的高手指点一下