This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. TPS65910A的39管脚 (GPIO_CKSYNC)输出的PMIC_GPIO信号到MPU的RTC_PORZ管脚,,在PMIC尚未实现初始化是不能输出高电平的嘛,其默认配置是输入,这样AM3358岂不是一直启动不了么?
Steven:不会,你注意看一下PMIC_GPIO的信号来源于VRTC,而VRTC是由VBAT 5V进来通过TPS71718产生的,所以这里PMIC_GPIO的拉高动作来源于VRTC来源于5V输入,不依赖于TPS65910.另外注意一下,那个TPS65910的39管脚是没接的,电阻DNI,这个GPIO_CKSYNC是用作时钟同步的,当前设计中并未使用。
2. 你别把PMIC输出的VRTC搞混了,那个输出在这个原理图里面的标号是VPMIC_VRTC,这个用作了boot模式的设置。和那些标号为VRTC的目前没有连在一起。
那么还必须用到一个电源TPS71718来输出VRTC? 而VRTC也用不了多少电流啊,所以我能不能直接用PMIC芯片TPS65910A来输出VRTC信号给MPU,而不用另外的电源来单独输出VRTC电源?
是这样,当时那个TPS65910的VRTC的输出电流太低了,不足以驱动AM335x的RTC模块,所以加了一个TPS71718来驱动,后来TPS65910做了更新,就没有这个问题可以直接接RTC了。
你可以参考:http://www.ti.com/product/AM3358/technicaldocuments#doctype6中的TPS65910x user guide
hi ,Steven
我想用TPS65910电源管理控制AM335x系统开关机。看芯片上33脚有个pwron。不知道这个pwron是怎么使用的,系统开机的时候是需要将pwron脚拉低,PMU上各个电源才能启动吗?还是需要另外设计一套开机电路?
电压路数不一样的,都可以给AM335x供电,TPS65217带charger。
你好!如果不使用AM3358内部的RTC模块,当使用TPS65910A3A1电源管理芯片时,是不是也可以不需要额外加一路单独的LDO,直接采用其他任意的一路1.8v电压给VDDS_RTC供电?