This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助 Unable to read "uImage" from mmc 0:1 for OMAP-L138

Other Parts Discussed in Thread: OMAP-L138

我使用的是OMAP-L138的板子,TI 提供的开发包OMAPL138 DVSDK 4.02 Installer.

在DVSDK 4.02 的包里编译了linux 2.6.33内核,copy to MMC上运行。出现如下错误:

请各位高手帮忙解决以下

U-Boot 2009.11 (Jan 13 2011 - 01:05:37)

I2C:   ready
DRAM:  64 MB
MMC:   davinci: 0
In:    serial
Out:   serial
Err:   serial
ARM Clock : 300000000 Hz
DDR Clock : 132000000 Hz
Net:   Ethernet PHY: GENERIC @ 0x00

Hit any key to stop autoboot:  0
reading boot.scr

248 bytes read
## Executing script at c0600000
reading uImage

** Unable to read "uImage" from mmc 0:1 **
Wrong Image Format for bootm command
ERROR: can't get kernel image!