仿真器初次连时总显示线没连好或没有时钟,放一会儿再连接就好了,使用一会儿又出现了原来的问题,这是怎么回事儿啊?太诡异了,请专家指教
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
仿真器初次连时总显示线没连好或没有时钟,放一会儿再连接就好了,使用一会儿又出现了原来的问题,这是怎么回事儿啊?太诡异了,请专家指教
我用的是是自己设计的硬件板,仿真器类型为TDS560,报错时显示的问题如下:
D:\CCStudio_v3.3\cc\bin>D:\CCStudio_v3.3\cc\bin\xdsreset.exe -p0 -fD:\CCStudio_v
3.3\cc\bin\TDS560USB_PLUS.cfg
-----[Print the reset-command software log-file]-----------------------------
This utility has selected an XDS560 class product.
This utility will load the program 'TDS560USB_PLUS.out'.
This utility will operate on port address '0'.
The controller does use a programmable FPGA.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver.
The value is '-182' (0xffffff4a).
The title is 'SC_ERR_CTL_CBL_BREAK_NEAR'.
The explanation is:
The controller has detected a cable break that is near-to itself.
The user must connect the cable/pod to the controller.
D:\CCStudio_v3.3\cc\bin>PAUSE
请按任意键继续. . .
请指点,万分感谢~!
解决了,的确释仿真器接头有问题,无意中发现的,汗哪~