This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ubi文件系统问题



ubi文件系统问题,麻烦解答一下,谢谢。

问题一

[    1.257385] UBI: attaching mtd7 to ubi0

[    1.537597] UBI: MTD device size:            50 MiB

[    1.542694] UBI: number of good PEBs:        100

[    1.547515] UBI: number of bad PEBs:         0

 

[    3.200927] UBI error: do_sync_erase: cannot erase PEB 99, error -5

[    3.207489] UBI error: erase_worker: failed to erase PEB 99, error -5

[    3.214202] UBI: mark PEB 99 as bad

//MTD 控件的倒数第二个PEB;原先为30M(60PEB),此时打印擦除PEB 59失败。

为何擦除块会跟着调整大小跑?

 

[    3.850250] nand_erase_nand: attempt to erase a bad block  at page 0x00002800

[    3.857666] UBI error: do_sync_erase: cannot erase PEB 61, error -5

[    3.864227] UBI error: erase_worker: failed to erase PEB 61, error -5

[    3.870941] UBI: mark PEB 61 as bad

 

[    3.874633] UBI warning: erase_worker: last PEB from the reserved pool was used

 

问题二

mount: mounting /dev/mtdblock9 on /usr_data failed: Invalid argument

 

[    4.199310] UBI: VID header offset:          2048 (aligned 2048)

[    4.205566] UBI: data offset:                4096

[    4.212005] UBI error: validate_ec_hdr: bad VID header offset 4096, expected 2048

 

文件系统分为两部分,ubi.img和sys_data.img,第一部分的VID header offset是在u-boot的evnpara中定义的,请问第二部分的VID header offset在哪儿定义的?

 

 

Flash分区如下:

[    1.083770] 0x000000000000-0x000000080000 : "SPL"

[    1.090148] 0x000000080000-0x000000100000 : "SPL.backup1"

[    1.097167] 0x000000100000-0x000000180000 : "SPL.backup2"

[    1.104125] 0x000000180000-0x000000200000 : "SPL.backup3"

[    1.111022] 0x000000200000-0x000000400000 : "U-Boot"

[    1.117584] 0x000000400000-0x000000480000 : "U-Boot Env"

[    1.124389] 0x000000480000-0x000000980000 : "Kernel"

[    1.131286] 0x000000980000-0x000003b80000 : "File System"       //ubi.img分区

[    1.143371] 0x000003b80000-0x00000ef80000 : "App data"         //sys_data.img分区

[    1.168640] 0x00000ef80000-0x000040000000 : "User data"

 

制作ubi相关定义如下:

mkubi.sh

sudo mkfs.ubifs -r ../rootfs -F -o ubifs.img -m 4096 -e 516096 -c 50

sudo ubinize -o ubi.img -m 4096 -p 512KiB -s 512 -O 4096 rootfs.cfg

 

rootfs.cfg

vol_size=24MiB

附部分串口记录:

[    2.927642] UBIFS: free space fixup complete

[    3.059417] UBIFS: mounted UBI device 0, volume 0, name "rootfs"

[    3.065795] UBIFS: file system size:   22708224 bytes (22176 KiB, 21 MiB, 44 LEBs)

[    3.073699] UBIFS: journal size:        5160960 bytes (5040 KiB, 4 MiB, 10 LEBs)

[    3.081329] UBIFS: media format:       w4/r0 (latest is w4/r0)

[    3.087402] UBIFS: default compressor: lzo

[    3.091674] UBIFS: reserved for root:  0 bytes (0 KiB)

[    3.105102] VFS: Mounted root (ubifs filesystem) on device 0:13.

[    3.113067] Freeing init memory: 988K

[    3.151397] nand_erase_nand: attempt to erase a bad block at page 0x00002700

[    3.168457] nand_erase_nand: attempt to erase a bad block at page 0x00002700

[    3.183349] nand_erase_nand: attempt to erase a bad block at page 0x00002700

[    3.203765] nand_erase_nand: attempt to erase a bad block at page 0x00002700

[    3.211120] UBI error: do_sync_erase:cannot erase PEB 59, error -5

[    3.217681] UBI error: erase_worker: failed to erase PEB 59, error -5

[    3.224426] UBI: mark PEB 59 as bad

[    3.228088] UBI: 1 PEBs left in the reserve

Mounting /proc and /sys

Starting the hotplug events dispatcher mdev

Mounting filesystems

[    3.797668] nand_erase_nand: attempt to erase a bad block at page 0x00002200

[    3.815277] nand_erase_nand: attempt to erase a bad block at page 0x00002200

[    3.824645] nand_erase_nand: attempt to erase a bad block at page 0x00002200

[    3.851196] nand_erase_nand: attempt to erase a bad block at page 0x00002200

[    3.858642] UBI error: do_sync_erase: cannot erase PEB 49, error -5

[    3.865173] UBI error: erase_worker: failed to erase PEB 49, error -5

[    3.871887] UBI: mark PEB 49 as bad

[    3.875610] UBI warning: erase_worker: last PEB from the reserved pool was used

mount: mounting /dev/mtdblock9 on /usr_data failed: Invalid argument

 

  • 用的是什么型号的NAND FLASH,感觉参数设的不对啊

  • 最好把linux启动部分的log也贴上来

    这个大多是参数被设置好,ubifs制作的有问题

  • 1、NAND相关信息

    NAND FLASH :Micron MT29F8G08ABABAWP

    Page size x8:4320 bytes(4096 + 224 bytes)

    Block size:128 pages(512K + 28K bytes)

    Plane size:2 planes x 1024 blocks per plane

    Device size:8Gb:2048 Blocks

    Minimum required ECC:4-bit ECC per 540 bytes of data

    2、文件系统制作相关信息

    1)ubi.img

    mkubi.sh:

    sudo mkfs.ubifs -r ../rootfs -F -o ubifs.img -m 4096 -e 516096 -c 99

    sudo ubinize -o ubi.img -m 4096 -p 512KiB -s 4096 -O 4096 rootfs.cfg

    rootfs.cfg:

    [ubifs]

    mode=ubi

    image=ubifs.img

    vol_id=0

    vol_size=40MiB

    vol_type=dynamic

    vol_name=rootfs

    vol_flags=autoresize

    2)sys_data.img

    mksys.sh:

    sudo mkfs.ubifs -r ../rootfs/sys_data -F -o sys_datafs.img -m 4096 -e 516096 -c 300

    sudo ubinize -o ubi.img -m 4096 -p 512KiB -s 4096 -O 4096 sys_data.cfg

    sys_data.cfg:

    [ubifs]

    mode=ubi

    image=sys_datafs.img

    vol_id=0

    vol_size=144MiB

    vol_type=dynamic

    vol_name=sys_data

    vol_flags=autoresize

    3、NAND FLASH分区信息

    [    1.083770] 0x000000000000-0x000000080000 : "SPL"

    [    1.090148] 0x000000080000-0x000000100000 : "SPL.backup1"

    [    1.097167] 0x000000100000-0x000000180000 : "SPL.backup2"

    [    1.104125] 0x000000180000-0x000000200000 : "SPL.backup3"

    [    1.111022] 0x000000200000-0x000000400000 : "U-Boot"

    [    1.117584] 0x000000400000-0x000000480000 : "U-Boot Env"

    [    1.124389] 0x000000480000-0x000000980000 : "Kernel"

    [    1.131286] 0x000000980000-0x000003b80000 : "File System"       //ubi.img分区

    [    1.143371] 0x000003b80000-0x00000ef80000 : "App data"         //sys_data.img分区

    [    1.168640] 0x00000ef80000-0x000040000000 : "User data"

    4、u-boot中paraevn 参数信息

    root=ubi0:rootfs rw ubi.mtd=7,4096 noinitrd rootfstype=ubifs rootwait=1 ip=none

    5、启动信息见附件。

  • Jian Zhou , 麻烦帮忙看看这个问题呢。

  • 用这个命令试下:

    mkfs.ubifs -F -q -r ../rootfs -F -o ubifs.img -m 4096 -e 522240 -c 4095 -o ubifs.img

  • 您好!jian zhou ,

      nor flash只有32M,现在已经可以启动了。请问怎么可以下载到一个小点文件系统,以便烧写到nor flash中呢!

  • 我们的SDK本身就带有一个10几兆的小文件系统,你可以试下。

  • 另外看你说的Nor Flash可以启动了,是UbiFS可以挂载上了么?你修改了哪些参数可以共享下么?

  • 您好!我说的可以启动的意思是 :可以从nor flash 中的uboot起来,也可以引导nor flash内存储的内核了。挂在tf卡上的文件系统是可以的,但是没有找到可以烧写进nor flash的文件系统。

    还有您说的那个十几兆的文件系统方便发给我一下吗,我找到的最小是二十多兆,谢谢您!

    我的邮箱是874706726@qq.com

  • 你有下载我们官方的SDK么?里面有带2个压缩好的文件系统,一个200多M,另外一个十几兆