This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: Errors:unresolved symbol GPIO

Part Number: TMS320C6748


你好,我是一个DSP新手,正尝试运行一些案例时遇到一点困难,已经该网站TMDSLCDK6748 开发套件 | TI.com.cn安装了CCS_v9和最新版的ti-processor-sdk-rtos-omapl138-lcdk-06.03.00.106-Windows-x86-Install.exe,均安装在默认路径。

当我对工程右键进行build project时,报出以下错误,请问专业人士这些错误代表什么意思,该如何去解决?谢谢。

undefined first referenced
symbol in file
--------- ----------------
GPIOBank6Pin12PinMuxSetup ./gpioCardDetect.obj
GPIODirModeSet ./gpioCardDetect.obj
GPIOPinWrite ./gpioCardDetect.obj
PSCModuleControl ./gpioCardDetect.obj

error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "led2.out" not built

>> Compilation failure
makefile:149: recipe for target 'led2.out' failed
gmake[1]: *** [led2.out] Error 1
makefile:145: recipe for target 'all' failed
gmake: *** [all] Error 2

**** Build Finished ****