This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: SPI boot nor flash

Part Number: TMS320C6657


您好!

我们现在正在使用的是C6657的自制版,想采用SPI nor flash的形式进行boot,nor flash用的赛普拉斯的S25FS512,测试过读写没有问题

现在工程中程序是单核的带有sys/bios的,并且没有将程序段或者数据段放入DDR,map的配置如下:

主要都放在了LL2和MSMC中。

生成出来的.out文件比较大,达到了7M多,在论坛上找到了8838.SPI_Bootloader的工具。8838.SPI_Bootloader.zip

我将.out文件修改成simple.out后,运行后,提示我在将.btbl转换为.i2c时,输入数据过大,无法转换

尝试过将.rmd里length = 0x1000000,字节数大于我的.out文件,但结果依然一样,在转换为.i2c时失败。

请问,我需要怎么做才能将我的.out文件给通过工具链生成出待烧写的.dat或者.bin文件呢?

是否还有其他版本的工具链可以解决这一问题呢?

希望得到解答

谢谢!