This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J784S4XEVM: 开发板出现故障,无法工作。

Part Number: J784S4XEVM

上电之后,指示灯就亮,散热器不工作,开关不好使,拨动开关指示灯没有变化,如图所示,怎么解决?

  • 请看一下电源是否满足手册上的要求。
    2.1 Power Input

    A power supply is not included with the EVM and must be purchased separately.

    External Power Supply or Power Accessory Requirements:

    • Output Voltage: 24-48 VDC

    • Output Power Capacity: 100-160 W (depending on use case and connected peripherals)

    • Efficiency Level V

    Note

    TI recommends using and external power supply or power accessory which complies with the applicable regional safety standards such as (by example) UL, CSA, VDA, CCC, PSE, etc.
    https://www.ti.com/lit/ug/spruj62/spruj62.pdf

    拨动开关指示灯没有变化

    是Power Control [SW1] with LED for Status [LD7][LD8][LD9]这几个指示灯吗?

  • 电源满足要求,是PWR LED   FAULT LED   LD7  LD8  LD9  LD10这几个指示灯

  • 那可能板子有问题了,请按照以下方式联系客户支持部门的技术部门,会有技术客服为您提供帮助。

    • 打开链接https://ticsc.service-now.com/csm
    • 点击申请新的支持下面的提交申请按钮
    • 在新打开的窗口中点击技术帮助下面的创建案例按钮
    • 在打开的表格中您可以使用中文描述您的问题并且递交。递交申请时,请您提及以下信息:
      • Ti.com购买订单号
      • 需要技术鉴定EVM是否存在质量问题
      • 您是否使用免费邮箱注册myti账号