Part Number: AM3358
linux kernel version :3.0
CAN frame :DCAN
whether this version is related to the interrupt controller
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The Linux kernel version 3.0 does not have explicit support for the AM335X interrupt controller. However, it should still work with the interrupt controller on the AM335X SoC. The delay you are experiencing might be due to other factors such as interrupt handling in the kernel or the specific implementation of the interrupt controller driver. Upgrading to a newer version of the Linux kernel that provides better support for the AM335X interrupt controller might help resolve this issue.
Regards,
Gary