GPMC接口为啥有GPMC_WAIT0 GPMC_WAIT1两个wait 信号?他们的区别是什么?我再TRM中没看到
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
GPMC接口为啥有GPMC_WAIT0 GPMC_WAIT1两个wait 信号?
GPMC_WAIT0和GPMC_WAIT1是GPMC(General-Purpose Memory Controller)接口中的等待信号,用于处理外部设备的读写延迟。
他们的区别是什么?
区别于作用的时间点不同
GPMC_WAIT0:在读取数据时,GPMC_WAIT0信号用于等待外部设备的读取延迟。当外部设备需要更多时间来准备数据时,GPMC可以使用GPMC_WAIT0信号等待。
GPMC_WAIT1:在写入数据时,GPMC_WAIT1信号用于等待外部设备的写入延迟。当外部设备需要更多时间来接收和处理数据时,GPMC可以使用GPMC_WAIT1信号等待。
您好,如果您已经将P7引脚用作了gpmc_clk,而N1引脚用作了gpmc_advn_ale,那么gpmc_wait1可能已经被占用,无法再用于其他功能。
在GPMC(General-Purpose Memory Controller)接口中,gpmc_wait1通常用于读取等待。如果您不使用gpmc_wait1,而且您的FPGA足够快,您可以尝试不使用读取等待信号。但是请注意,如果您的系统中存在读取延迟或其他因素可能导致读取冲突,那么使用读取等待信号是一个较为安全和可靠的做法。
另外,gpmc_wait0通常用于写入等待。在GPMC接口中,读取和写入通常需要分别使用不同的等待信号。因此,如果您需要进行读取和写入操作,最好使用gpmc_wait0和gpmc_wait1分别作为读取和写入的等待信号。
您好,
gpmc_wait0和gpmc_wait1通常用于写入和读取的等待信号,分别对应写入等待和读取等待。这两个信号通常是分开使用的,以确保读取和写入操作的稳定性和正确性。
gpmc_wait0用于写入等待,在写入数据时,如果写入缓冲区已满或者写入操作还未完成,gpmc_wait0信号将保持高电平,直到写入操作完成。
gpmc_wait1用于读取等待,在读取数据时,如果读取缓冲区为空或者读取操作还未完成,gpmc_wait1信号将保持高电平,直到读取操作完成。
因此,为了确保读取和写入操作的稳定性和正确性,通常建议将gpmc_wait0用作写入等待,将gpmc_wait1用作读取等待。这样可以避免读取和写入操作之间的冲突。