This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我在使用AM3517的过程中,发现机器突然死机了,终端显示如下信息,不停的打印,不知道为什么,请问一下,有什么方法可以解决这个问题,我用的是TI官方提供的DEMO包。
LayMgr.cpp: Layout Manager successfully initialized to 1
MSIM: IM_ReadRegistry read KB 5
Explorer(V2.0) taskbar thread started.
NDISPWR:: Found adapter [SMSC91181]
NDISPWR:: Found adapter [EMAC1]
M 132,819 130,845 -2,26M 128,846 121,867 -7,21Write: Attempts = 2
Write: Attempts = 2
Write: Attempts = 2
M 140,188 133,294 -7,106Read: Attempts = 2
Read: Attempts = 3
Read: Attempts = 4
Read: Attempts = 5
WARN: I2C: Read failed (slave addr=0x4B, register=0x00000000)
Write: Attempts = 2
Write: Attempts = 3
Write: Attempts = 4
Write: Attempts = 5
WARN: I2C: Write failed (SA=0x4B, register=0x00000000)
Write: Attempts = 2
Write: Attempts = 3
Write: Attempts = 4
Write: Attempts = 5
WARN: I2C: Write failed (SA=0x4B, register=0x00000000)
Read: Attempts = 2
Read: Attempts = 3
Read: Attempts = 4
Read: Attempts = 5
WARN: I2C: Read failed (slave addr=0x4B, register=0x00000000)
请您明确下一下问题:
1. 您所使用的开发部是否是ti原厂提供的开发板,是哪一款?
2. 您所使用的demo sdk是哪个版本?
3. 在什么情况下导致死机?