Hi 各位專家:
你好, 想請教 我在am3358 的 debug consle 上面輸入超過61個字元後, console 並不會新增下一行, 而是同一行覆蓋之前的文字
在同一個條件下我在非TI AM3358的板子上並不會有這樣的問題. 讓我再輸入指令的時候十分的困擾
想請問專家可以解答一下我該如何讓他自動換行

感謝
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi 各位專家:
你好, 想請教 我在am3358 的 debug consle 上面輸入超過61個字元後, console 並不會新增下一行, 而是同一行覆蓋之前的文字
在同一個條件下我在非TI AM3358的板子上並不會有這樣的問題. 讓我再輸入指令的時候十分的困擾
想請問專家可以解答一下我該如何讓他自動換行

感謝
请问使用的是最新的processor SDK吗?
https://www.ti.com/tool/PROCESSOR-SDK-AM335X
请问同样的ti-processor-sdk-linux-am335x-evm-08.02.00.24 kernel在非TI AM3358的板子上是可以换行的,但是在TI的EVM板上不能换行是吗?请问用的是哪块EVM板?
你好 非TI AM3358 的板子 kernel 並不是ti-processor-sdk-linux-am335x-evm-08.02.00.24 我只是想陳述我的console 環境應該是沒問題的
而在TI 的板子上 我運行ti-processor-sdk-linux-am335x-evm-08.02.00.24 在 AM3358 GP EVM 是無法換行的
我使用ti-processor-sdk-linux-am335x-evm-08.02.00.24
並無做任何kernel 的修改並燒錄官方預設rootfs (tisdk-default-image-am335x-evm.tar.xz)
謝謝您的回覆
请看下面e2e工程师的回复。
Can you have them echo the value of "$COLUMNS" in both of these environments? Certain combinations of terminal emulators and serial monitors can misbehave and potentially misreport / ignore certain terminal standards.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1269805/am3358-debug-console-not-start-a-new-line
请看下面e2e工程师最新的回复。
This is because by default our terminal uses the settings transmitted by the serial console to initialize line and column count (often referred to as terminal geometry). This is expected default behavior for most modern terminals, however serial terminals are a little special. They respect the initialization but there is no way to transmit resize events. As such, if you resize there terminal emulator window you will need to reissue the "resize" command to reload terminal geometry.
The discrepancy comes from some vendors choosing to lock the serial console geometry to an older standard like 80x23. In which case you're fine until you resize the window smaller than that. (If you're curious about how terminal resize events work please see the following: https://www.gnu.org/software/libc/manual/html_node/Miscellaneous-Signals.html). Unfortunately there's really not a nice, standard solution to this currently.